Part Number: DRA821U
Other Parts Discussed in Thread: DRA821
Dear Champs,
I learnt CAN data packet can be exchanged to linux of A72 core through IPC in below e2e.
My customer has used open CAN stack working on linux in other platform and they also want to use it in DRA821U, but the problem is there is no CAN linux driver for DRA821U.
Do you think it is possible to use CAN stack on linux of DRA821U A72 core while exchanging CAD data packet with Cortex-R5 core through IPC?
Their target is to process several CAN protocols like ISO-TP and SAE J1939-TP on Linux of A72 core to utilize open source CAN stack of linux.
Or, is there open source CAN stack supporting ISO-TP and SAE J1939-TP on Cortex-R5?
Thanks and Best Regards,
SI.