Other Parts Discussed in Thread: AM5728,
Hi,
The original project has been initialized on the dsp end of am5728 and configured as the rc end, and has been successfully applied. Currently the new project uses the am5708, the customer transplants the initialization code of the am5728 to this chip, and reads the controller during the training step, but it is not trained success.
1、AM5728 uses ccs6.13 am57xxPDK 1.0.4, and the arm side runs Linux without pcie driver
2、AM5708 uses ccs7.4.0 am57xxPDK 1.0.4, and the arm side runs Linux with pcie driver
use
Echo 1> /sys/devices/platform/44000000.ocp/44000000.ocp:axi@0/51000000.pcie/pci0000:00/0000:00:00.0/remove
Uninstalling the driver is also unsuccessful.
Please help give some suggestions.