Part Number: AM5728
Hi,
I'm looking for support, documentation or training to be able to use correctly VPS driver, focus on DSS, DISPC and HDMI.
I have used DisplayDSS project present in pdk (setup env, creatproject and also rebuild lib) thanks to scripts available.
But it's appears that this project is very huge and complex not useful to use.
I'm trying to setup a project just with parts that match with my use case (test case 11 of displayDSS project) .
Now I have an issue when I send IOCTL command to set DSS parameters (on validation VpsCore_dssValidateDssParams) dues to the size and format. I don't understand why.
Do someone help me on this topics ?
Here my strait forward code:
Vps_InitParams vpsInitPrms;
Fvid2_Handle dctrlHandle;
Bsp_PlatformSetPllFreq vPllCfg;
Bsp_PlatformVencSrc vencClkCfg;
int32_t retVal = FVID2_SOK;
// EDMA3_DRV_Handle hEdma;
// EDMA3_DRV_Result edmaResult = 0;
appPrint("\n hdmi dss task started...\r\n");
appPrint(" configuration match with DisplayDSS project -> test case : 11\r\n");
Fvid2_init(NULL);
VpsInitParams_init(&vpsInitPrms);
vpsInitPrms.irqParams.dssIrqNum = CSL_INTC_EVENTID_DSS_DISPC;
Vps_init(&vpsInitPrms);
//hEdma = edma3init(0, &edmaResult);
/* Create DCTRL handle, used for common driver configuration */
dctrlHandle = Fvid2_create(FVID2_VPS_DCTRL_DRV, VPS_DCTRL_INST_0, NULL, NULL, NULL);
vPllCfg.videoPll = BSP_PLATFORM_PLL_HDMI;
vPllCfg.pixelClk = 29232U * 4U;;
vPllCfg.chooseMaxorMinMN = (uint32_t) BSP_PLATFORM_VIDEO_PLL_CALC_MAX_MN;
retVal = Bsp_platformSetPllFreq(&vPllCfg);
if (retVal != FVID2_SOK) appPrint("\nConfiguring Pll Failed!!!\r\n");
vencClkCfg.outputVenc = BSP_PLATFORM_VENC_HDMI;
vencClkCfg.vencClkSrc = BSP_PLATFORM_CLKSRC_DPLL_HDMI;
retVal = Bsp_platformSetVencClkSrc(&vencClkCfg);
if (retVal != FVID2_SOK) appPrint("Setting Venc clock source Failed!!!\r\n");
retVal = Bsp_platformEnableHdmiPll(TRUE);
if (retVal != FVID2_SOK) appPrint("Enabling HDMI PLL Failed!!!\r\n");
appPrint(" hdmi vps/dctrl common configuration -> done...\r\n");
/* [IN] DispApp_create() l.562 DSS_main.c ------------------------------- */
/* [IN] DispApp_initParams() l.1414 DSS_main.c -------------------------- */
Hdmi_InstObj hdmiObj;
memset(&hdmiObj, 0x00, sizeof(Hdmi_InstObj));
hdmiObj.inDataFmt = FVID2_DF_YUV422I_YUYV;
hdmiObj.pitch[FVID2_YUV_INT_ADDR_IDX] = VpsUtils_align(1920U * 2U, VPS_BUFFER_ALIGNMENT);
hdmiObj.inWidth = 1920U;
hdmiObj.inHeight = 1080U;
hdmiObj.isFieldMerge = FALSE;
hdmiObj.inScanFormat = FVID2_SF_PROGRESSIVE;
hdmiObj.posx = 0U;
hdmiObj.posy = 0U;
hdmiObj.instId = VPS_DISP_INST_DSS_VID2;
hdmiObj.drvHandle = NULL;
Fvid2CbParams_init(&hdmiObj.cbPrms);
hdmiObj.cbPrms.cbFxn = &vps_dss_hdmi_cbFxn;
hdmiObj.cbPrms.appData = &hdmiObj;
VpsDispCreateParams_init(&hdmiObj.createPrms);
VpsDispDssParams_init(&hdmiObj.dssPrms);
hdmiObj.dssPrms.inFmt.chNum = 0U;
hdmiObj.dssPrms.inFmt.width = hdmiObj.inWidth;
hdmiObj.dssPrms.inFmt.height = hdmiObj.inHeight;
hdmiObj.dssPrms.inFmt.pitch[0U] = hdmiObj.pitch[0U];
hdmiObj.dssPrms.inFmt.pitch[1U] = hdmiObj.pitch[1U];
hdmiObj.dssPrms.inFmt.pitch[2U] = hdmiObj.pitch[2U];
hdmiObj.dssPrms.inFmt.fieldMerged[0U] = hdmiObj.isFieldMerge;
hdmiObj.dssPrms.inFmt.fieldMerged[1U] = FALSE;
hdmiObj.dssPrms.inFmt.fieldMerged[2U] = FALSE;
hdmiObj.dssPrms.inFmt.dataFormat = hdmiObj.inDataFmt;
hdmiObj.dssPrms.inFmt.scanFormat = hdmiObj.inScanFormat;
hdmiObj.dssPrms.inFmt.bpp = FVID2_BPP_BITS16;
hdmiObj.dssPrms.inFmt.reserved = NULL;
hdmiObj.dssPrms.tarWidth = hdmiObj.dssPrms.inFmt.width;
hdmiObj.dssPrms.tarHeight = hdmiObj.dssPrms.inFmt.height;
hdmiObj.dssPrms.posX = hdmiObj.posx;
hdmiObj.dssPrms.posY = hdmiObj.posy;
VpsDssDispcVidConfig_init(&hdmiObj.vidCfg);
hdmiObj.dssPrms.vidCfg = &hdmiObj.vidCfg;
/* ]IN[ DispApp_initParams() l.1414 DSS_main.c -------------------------- */
/* [IN] DispApp_configDctrl() l.889 DSS_main.c -------------------------- */
Vps_DctrlConfig dctrlCfg;
VpsDctrlConfig_init(&dctrlCfg);
dctrlCfg.useCase = VPS_DCTRL_USERSETTINGS;
dctrlCfg.numEdges = 0U;
/* Connect module video and gfx to hdmi */
// dctrlCfg.edgeInfo[dctrlCfg.numEdges].startNode =
// VPS_DCTRL_DSS_VID1_INPUT_PATH;
// dctrlCfg.edgeInfo[dctrlCfg.numEdges].endNode =
// VPS_DCTRL_DSS_HDMI_BLENDER;
// dctrlCfg.numEdges++;
dctrlCfg.edgeInfo[dctrlCfg.numEdges].startNode =
VPS_DCTRL_DSS_VID2_INPUT_PATH;
dctrlCfg.edgeInfo[dctrlCfg.numEdges].endNode =
VPS_DCTRL_DSS_HDMI_BLENDER;
dctrlCfg.numEdges++;
// dctrlCfg.edgeInfo[dctrlCfg.numEdges].startNode =
// VPS_DCTRL_DSS_VID3_INPUT_PATH;
// dctrlCfg.edgeInfo[dctrlCfg.numEdges].endNode =
// VPS_DCTRL_DSS_HDMI_BLENDER;
// dctrlCfg.numEdges++;
//
// dctrlCfg.edgeInfo[dctrlCfg.numEdges].startNode =
// VPS_DCTRL_DSS_GFX1_INPUT_PATH;
// dctrlCfg.edgeInfo[dctrlCfg.numEdges].endNode =
// VPS_DCTRL_DSS_HDMI_BLENDER;
// dctrlCfg.numEdges++;
dctrlCfg.edgeInfo[dctrlCfg.numEdges].startNode =
VPS_DCTRL_DSS_HDMI_BLENDER;
dctrlCfg.edgeInfo[dctrlCfg.numEdges].endNode =
VPS_DCTRL_DSS_HDMI_OUTPUT;
dctrlCfg.numEdges++;
dctrlCfg.vencInfo.modeInfo[0U].vencId = VPS_DCTRL_DSS_VENC_HDMI;
Fvid2ModeInfo_init(&dctrlCfg.vencInfo.modeInfo[0U].mInfo);
Fvid2_getModeInfo(&dctrlCfg.vencInfo.modeInfo[0U].mInfo);
dctrlCfg.vencInfo.modeInfo[0U].mInfo.scanFormat = FVID2_SF_PROGRESSIVE;
dctrlCfg.vencInfo.tiedVencs = 0U;
appPrint(" hdmi dctrlCfg configuration -> done...\r\n");
Vps_DssDispcOvlyPanelConfig panelCfg;
panelCfg.alphaBlenderEnable = 0;
panelCfg.backGroundColor = 0x00;
panelCfg.colorKeyEnable = 1;
/* Source transparency color key selected */
panelCfg.colorKeySel = VPS_DSS_DISPC_TRANS_COLOR_KEY_SRC;
panelCfg.deltaLinesPerPanel = 0;
panelCfg.transColorKey = 0x00;
panelCfg.vencId = VPS_DCTRL_DSS_VENC_HDMI;
// Vps_DctrlVencDivisorInfo vencDivisors;
//
// vencDivisors.vencId = VPS_DCTRL_DSS_VENC_HDMI;
// vencDivisors.divisorLCD = 1;
// vencDivisors.divisorPCD = 1;
Vps_DctrlOutputInfo vencOutput;
vencOutput.actVidPolarity = VPS_DCTRL_POLARITY_ACT_HIGH;
vencOutput.pixelClkPolarity = VPS_DCTRL_POLARITY_ACT_HIGH;
vencOutput.dvoFormat = VPS_DCTRL_DVOFMT_GENERIC_DISCSYNC;
vencOutput.hsPolarity = VPS_DCTRL_POLARITY_ACT_HIGH;
vencOutput.vsPolarity = VPS_DCTRL_POLARITY_ACT_HIGH;
vencOutput.dataFormat = FVID2_DF_RGB24_888;
vencOutput.videoIfWidth = FVID2_VIFW_24BIT;
vencOutput.vencId = VPS_DCTRL_DSS_VENC_HDMI;
/* This IOCTL should be called before SET_CONFIG_IOCTL */
retVal = Fvid2_control(dctrlHandle, IOCTL_VPS_DCTRL_SET_VENC_OUTPUT, &vencOutput, NULL);
if (retVal != FVID2_SOK) appPrint(" DCTRL Set Venc Output IOCTL Failed!!!\r\n");
retVal = Fvid2_control(dctrlHandle, IOCTL_VPS_DCTRL_SET_CONFIG, &dctrlCfg, NULL);
if (retVal != FVID2_SOK) appPrint(" DCTRL Set Config IOCTL Failed!!!\r\n");
retVal = Fvid2_control(dctrlHandle, IOCTL_VPS_DCTRL_SET_OVLY_PARAMS, &panelCfg, NULL);
if (retVal != FVID2_SOK) appPrint(" DCTRL Set OVLY Params IOCTL Failed!!!\r\n");
appPrint(" Send control commands (IOCTLs) to DCTRL for configuration -> done...\r\n");
/* [IN] DispApp_configDctrlPipe() l.1414 DSS_main.c --------------------- */
Vps_DssDispcOvlyPipeConfig *ovlpipecfg;
ovlpipecfg = &hdmiObj.ovlpipeconfig;
ovlpipecfg->pipeLine = hdmiObj.instId;
ovlpipecfg->globalAlpha = 0xFF;
/* Z-order is in order GFX - 3, VID3 -2 ,VID2 - 1 and VID1 - 0 */
ovlpipecfg->zorder = hdmiObj.instId;
ovlpipecfg->zorderEnable = 1;
ovlpipecfg->preMultiplyAlpha = 0;
retVal = Fvid2_control( dctrlHandle, IOCTL_VPS_DCTRL_SET_PIPELINE_PARAMS, ovlpipecfg, NULL);
if (retVal != FVID2_SOK) appPrint(" DCTRL Set Pipeline params IOCTL Failed!!!\r\n");
appPrint(" Send control commands (IOCTLs) to DCTRL Set pipeline -> done...\r\n");
/* ]IN[ DispApp_configDctrlPipe() l.1414 DSS_main.c --------------------- */
/* ]IN[ DispApp_configDctrl() l.889 DSS_main.c -------------------------- */
/* Create specific hdmi disp driver handler */
hdmiObj.drvHandle = Fvid2_create(FVID2_VPS_DISP_DRV, hdmiObj.instId, &hdmiObj.createPrms, &hdmiObj.createStatus, &hdmiObj.cbPrms);
retVal = hdmiObj.createStatus.retVal;
if ((NULL == hdmiObj.drvHandle) || (retVal != FVID2_SOK)) appPrint(" DSS Create Failed!!!\r\n");
vps_dss_hdmi_appPrintDispCreateStatus(&hdmiObj.createStatus);
retVal = Fvid2_control(hdmiObj.drvHandle, IOCTL_VPS_DISP_SET_DSS_PARAMS, &hdmiObj.dssPrms, NULL);
if (retVal != FVID2_SOK) appPrint(" DSS Set Params IOCTL Failed!!!\r\n");Thanks in advance
Quentin