This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4376: Project not created

Part Number: AM4376
Other Parts Discussed in Thread: AM4379

Hello ,

using below version

CCS10.4

sdk:ti-processor-sdk-rtos-am437x-evm-06.03.00.106-Windows-x86-Install

not able to generate project.

below is the error.

C:\ti\pdk_am437x_1_0_17\packages>pdkProjectCreate.bat AM437x idkAM437x little uart all arm C:\ti\pdk_am437x_1_0_17\packages
=========================================================================
Configuration:
SOC : AM437x
BOARD : idkAM437x
ENDIAN : little
MODULE : uart
PROJECT_TYPE : all
PROCESSOR : arm
PDK_SHORT_NAME : C:\ti\pdk_am437x_1_0_17\packages
=========================================================================
Checking Configuration...
Complete
=========================================================================
PDK_PARTNO : AM437
PDK_ECLIPSE_ID : com.ti.pdk.am437x
RTSC_PLATFORM_NAME : ti.platforms.evmAM437X
RTSC_TARGET : gnu.targets.arm.A9F
CCS_DEVICE : "Cortex A.AM4379.IDK_AM437X"
*****************************************************************************
Detecting all projects in PDK and importing them in the workspace C:\ti\pdk_am437x_1_0_17\packages\MyExampleProjects
Detected Test Project: UART_BasicExample_idkAM437x_armExampleProject
The system cannot find the path specified.
Copying macro.ini
The system cannot find the path specified.
0 file(s) copied.
Detected Test Project: UART_BasicExample_idkAM437x_armTestProject
The system cannot find the path specified.
Copying macro.ini
The system cannot find the path specified.
0 file(s) copied.
Project generation complete
*****************************************************************************

regards,

Vrund