Part Number: AMIC110
Hi,
My customer is evaluating AMIC110 with TI RTOS SDK v06.03.00.106.
They have below two questions.
Q1) Their system is working 24MHz SYSCLK.
They wants to configure DDR2 with 266MHz.
Where they should change the configuration in SDK code?
Q2) UART baud rate
Customer understood UART clock (48MHz) is 1/4 of 192MHz output from PER DPLL (ADPLLJ).
Where can customer configure PER DPLL output frequency and UART clock and baud rate(DLL and DLH) in SDK code?
Thanks and regards,
Koichiro Tashiro