This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J721E: PROCESSOR-SDK-J721E

Part Number: PROCESSOR-SDK-J721E

Not able to download the image into the flash?

Following the link:
https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-jacinto7/latest/exports/docs/linux/Foundational_Components/U-Boot/UG-QSPI.html

I have boooted the board to the u-boot using the SD card.

=> ping 192.168.1.2
am65_cpsw_nuss_slave ethernet@46000000: K3 CPSW: rflow_id_base: 2
link up on port 1, speed 1000, full duplex
Using ethernet@46000000 device
host 192.168.1.2 is alive

=> sf probe
SF: Detected mt35xu512aba with page size 256 Bytes, erase size 128 KiB, total 64 MiB
=> tftp ${loadaddr} tiboot3.bin
am65_cpsw_nuss_slave ethernet@46000000: K3 CPSW: rflow_id_base: 2
link up on port 1, speed 1000, full duplex
Using ethernet@46000000 device
TFTP from server 192.168.1.2; our IP address is 192.168.1.3
Filename 'tiboot3.bin'.
Load address: 0x82000000
Loading: T T T T T T T T T T
Retry count exceeded; starting again