Hi experts,
My customer is considering using the AM5706 in combination with the TPS659163.
Q1: Checking the following thread, there seems to be a Linux Driver (palmas-regulator.c) for TPS65917, am I right in understanding that this Driver can be used for TPS659163 as is?
Please let me confirm that it can also be used for AM5706 just to be sure.
URL:e2e.ti.com/.../am5716-tps65916-driver-support-am5716
Q2: If the driver needs to be modified, it would be very helpful if you could share information about the modifications.
For example, Migration Guide or something like that.
Q3: It would also be helpful if you could share information on how to integrate the driver into U-Boot.
Best regards,
O.H