This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMAG 5170UEVM - I do not manage to connect to device on Mac OS



Dear Team,

Unfortuantely, I failed to get the TMAG 5170UEVM board connected to my Mac. It seems that it has been detected by the OS, but I always get the same error message when trying to connect. I did the FW upload which completed successfully. Could you please help me?

USB 3.0 Bus:

  Host Controller Driver: AppleUSBXHCISPT

  PCI Device ID: 0xa12f 

  PCI Revision ID: 0x0031 

  PCI Vendor ID: 0x8086 

Generic Bulk Device:

  Product ID: 0x00ab

  Vendor ID: 0x1cbe  (Texas Instruments - Stellaris)

  Version: 1.00

  Serial Number: 12345678

  Speed: Up to 480 Mb/s

  Manufacturer: Texas Instruments

  Location ID: 0x14600000 / 29

  Current Available (mA): 500

  Current Required (mA): 500

  Extra Operating Current (mA): 0