This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
The edgeai-yolov5 using command: python train.py --data coco.yaml --cfg yolov5s6.yaml --weights '' --batch-size 64
Trained network runs/train/exp2/weights/best.pt
Convert it to onnx using the command below: python export.py --weights pretrained_models/yolov5s6_640_ti_lite/weights/best.pt --img 640 --batch 1 --simplify --export-nms --opset 11
Issue: The onnx is generated without the corresponding .prototxt file being generated in sync. The customer would like to know how to generate the prototxt file. Without the prototxt file, the xx.bin file cannot be generated using the edgeai-tidl-tool.
Could you help check this case? Thanks.
Best Regards,
Cherry
Hello Cherry,
Apologies for the delayed response.
If you are following this github https://github.com/TexasInstruments/edgeai-yolov5, then the prototxt files can be found in the compressed files here: https://github.com/TexasInstruments/edgeai-yolov5/tree/master/pretrained_models/modelartifacts/8bits
Regards,
Takuma
Hi Takuma,
Thanks for your response.
The customer has checked the file you provided and did not get the answer, customer would like to know how this prototxt file was generated and how the numbers were calculated.
Thanks and Best Regards,
Cherry
Hi Takuma,
May I know is there any updates about the question above? Thanks.
Best,
Cherry
Hi Cherry,
I have forwarded this question to the developer of edgeai-yolov5
He should be replying soon.
Regards,
Manu
While we are waiting for Debapriya Maji to respond, you may look here for example prototxt files for yolov5:
https://github.com/TexasInstruments/edgeai-yolov5/tree/master/pretrained_models/models
Specifically, is this the model that you are looking for?
Note: the .link files are text files. If you open it, you can get the url for the actual file and you can download it using wget.
Regards,
Hi Cherry,
Will you please share the onnx model that you have exported and the error you are getting while using the shared prototxt for import.
Regards, Debapriya
Hi dear all,
Thanks for your support and I have updated to the customer, if there is any new feedback I will reach you ASAP.
Thanks again!
Best Regards,
Cherry
Hi,
The updates are as follows:
When using edgeai-tidl-tools to convert the semantic split network onnx file into bin, run the command python onnxrt_ep.py -c. The generated .bin file performs very poorly on TDA4. Warning during conversion: Warning: [TIDL_E_DATAFLOW_INFO_NULL] ti_cnnperfsim.out fails to allocate memory in MSMC. Please look into perfsim log. This model can only be used on PC emulation, it will get fault on target.
There is also a something that looks abnormal: Substitute string tidl_net_ not Found
Could you help check what's happening?
Thanks and Best Regards,
Cherry
Hi Cherry,
It will be great if the ONNX model and the corresponding prototxt can be shared.
Regards, Debapriya
Hi Debapriya,
Please check if these works.
Thanks and Best Regards,
Cherry
Hi Debapriya,
May I know is there any feedback regarding the info above?
Thanks and Best Regards,
Cherry
Hi Cherry,
I tried this model and it is working fine. These models and prototxt were shared by TI and was validated. Now, based on the pytorch and ONNX version, the prototxt may have to be changed.
Hence, if you can share the exact model and prototxt that will help..
Regards, Debapriya
HI Cherry,
The first error comes during calibration when the model run an epoch of floating point inference. That should be fine. It will not come after the calibration error.
The second warning can also be ignored.
I think the issue is in defining the correct prototxt. If the prototxt is not defined correctly, some layers will go to ARM and result in high latency.
Regards, Debapriya
Hi Debapriya,
Thanks for your kind support again!
The customer would like to know how to ensure the date of prototxt, is there any related documents?
Thanks and Best Regards,
Cherry
Hi,
You can pull the latest code from https://github.com/TexasInstruments/edgeai-yolov5. While exporting an ONNX model, it exports the corresponding prototxt file as well. This will probably be helpful.
Regards, Debapriya