Hi,
using TMDSICE3359 i'm trying to flash an application in SPI memory.
I've connected pins 1 and 2 of J5 and i've launched "isdk_spi_flasher.out" using CCSv6 : after that i have selected, from the console, Flash --> App [0x20000] and i've uploaded my ".bin" file [from the menu Tools-->Load Memory] at the address 0x80100000 as written in console.
After this upload i've selected "0" but the "flash write operation" has not started. Why? Is it correct to upload the ".bin" file from Tools-->Load Memory?