Part Number: 66AK2G12
Hi experts,
The original thread was locked with no updates, so I'll repost it.
Please tell me about the ASRC built into the 66AK2G12.
Q1:Is it correct that the data input/output to ASRC must go through TeraNet_DMA? Or, is it possible to input data directly from McASP to ASRC, process it, and then output it again via ASRC in McASP?
Q2:For example, is it possible to take a signal at 96.1kHz from McASP, process it at 96kHz internally via ASRC, and then output it at 96.1kHz via ASRC again?
Q3:According to "11.1.3.3 ASRC Data Interface and Formats" in TRM, is it correct to truncate the MSB of a 32-bit input from McASP for a maximum 24-bit input/output? Or is it LSB truncation?
Our customer is starting to design a motherboard (audio I/O, etc. except K2G and C6657) for evaluation. So, I would like to know if I need a separate external ASRC or not, and I would appreciate your help.
If you have difficulty answering the part about ASRC, or if you can answer offline, please let us know which one.
Best regards,
O.H