This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Sometimes our board with TDA4VM SoC can't work on the 2133MHz DDR.
We need to locate this problem and it's need to disable the LFSR DQ training feature.
Please provide the method to disable the LFSR DQ training feature, thanks.
Hi,
Please see the post below. The parameter PHY_WDQLVL_PATT_* contains the patterns used during write data training. Bit 0 corresponds to LFSR.
Regards,
Kevin
hi expert
Modify as shown in the link TDA4VM Running ok
when i read the TRM and found LFSR training pattern can be use work around and ti are continue optimize setting
and ti do not suggerst customer disable TDA4VM periodic writing DQ training ,it just for debug and not used for mass product
my question is
What will be the impact of closing LFSR DQ
If it is a workaround , when will the mass production solution be resolved
Regards
yao