Part Number: TDA4VM
-1-
Are you aware of any threads where calculation of DMIPS for an algorithm is discussed for TDA4VM ?
-2-
I see in TRM “One dual-core 64-bit Arm Cortex-A72 microprocessor subsystem at up to 2.0 GHz and up to 24K DMIPS”
24K DMIPS is for both A72 cores together right?
-3-
I see that for A72 from Arm specs it is 7.3 DMIPS/MHz, so TDA4VM configuring at 2GHz, it should be 7.3x2000(2GHz=2000MHz)x2(2 A72 cores)=29,200 DMIPS/Mhz= 29.2K DMIPS/MHz , please clarify