Part Number: DRA821U
I'm working with a customer that is considering using the WKUP_UART as their (backup) boot device, as opposed to the MCU_UART. More background in these answered E2E questions:
It looks like the DMSC can (optionally?) use WKUP_UART to print logs. That leads to a few questions:
- If printing DMSC logs on WKUP_UART is optional, how is this disabled/enabled?
- If the DMSC logging to WKUP_UART is disabled, can WKUP_UART be used as a boot device and/or by the user application without later interference from the DMSC?
Thanks,
Stuart