This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Is there any solution for early boot?

Part Number: TDA4VM
Other Parts Discussed in Thread: TDA2

Is there any solution for early boot?


I'm checking up TDA4VM PSDKRA and PSDKLA.
I want the same as early boot solution in VISION SDK of TDA2.

The below functions are that I applied in TDA2.
1. Receive video from camera.
2. Make and display surround view.
3. Start H.264 encoding and store the encoded data in DRAM during booting.
4. Run QT after booting linux and display QT gui using DispDistSrc link.

The functions 1, 2 and 3 are executed in 4 or 5 seconds.
Of course, these are executed in IPU before booting linux.

If there are solution, patch, or guide for above functions, let me know that.

Best Regards,
Yousik Kim.