Hi,
I am trying the new 8.02 SDK original image
But find the Weston has error and the desktop GUI cannot show up. the Weston log is as below
root@j7-evm:/var/log# cat weston.log
Date: 2022-03-23 UTC
[23:52:48.082] weston 8.0.0
wayland.freedesktop.org
Bug reports to: gitlab.freedesktop.org/.../
Build: 8.0.0
[23:52:48.082] Command line: weston --idle-time=0
[23:52:48.083] OS: Linux, 5.10.100-rt62-g204ec708dc, #1 SMP PREEMPT_RT Thu Mar 24 00:09:37 UTC 2022, aarch64
[23:52:48.083] Using config file '/etc//weston.ini'
[23:52:48.087] Output repaint window is 7 ms maximum.
[23:52:48.090] Loading module '/usr/lib/libweston-8/drm-backend.so'
[23:52:48.103] initializing drm backend
[23:52:48.104] logind: not running in a systemd session
[23:52:48.104] logind: cannot setup systemd-logind helper (-61), using legacy fallback
[23:52:48.180] using /dev/dri/card1
[23:52:48.180] DRM: supports universal planes
[23:52:48.180] DRM: supports atomic modesetting
[23:52:48.180] DRM: supports picture aspect ratio
[23:52:48.181] Loading module '/usr/lib/libweston-8/gl-renderer.so'
(1093) PVR:(Error): PVRDRICreateScreenImpl: Failed to open render device node [ :171 ]
MESA-LOADER: failed to open kms_swrast (search paths /usr/lib/dri)
failed to load driver: kms_swrast
MESA-LOADER: failed to open swrast (search paths /usr/lib/dri)
failed to load swrast driver
[23:52:48.396] failed to initialize egl
[23:52:48.469] fatal: failed to create compositor backend
Internal warning: debug scope 'drm-backend' has not been destroyed.
Similar stuff happened in the last SDK release!
But this time seems have the new problem!
Have you even try to boot up your own default image before release?
Since these Weston bugs and malfunction are so obvious and immediate after the boot up.
Thanks!