Dear TI Team ,
I have created new thread with the continuation of Old Query link as by mistakenly I have set this thread to "resolved".
Q1 . Ref to Old Query link ,can you please give more details about your statement i.e "deny_list is mainly provided as a debugging option, it may not bring value in real application."==> is that mean , we cannot use this option manualy for real time project or choosing the layers which are offloaded to TIDL is decided by compiler automatically ?
Q2. It would be good , if you can give clear steps to run inference on target , ie how we need to create SD Card , commands/scripts which need to call during target inference considering semantic segmentation as an example
Q3.Suppose , if we have model and in which one of the layer should be executed on the MPU and rest all on target , Will there be any separate deliverables for TIDL and MPU or single ? in case of 2 , how to differentiate ?how to use these generated deliverables in the main application of the project which includes preprocessing , post processing.....model as per project specification written using TIDL API's
Thanks