This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-TDA4VM: Acquiring IP address of wireless access point for remote connection to device without use of display (SCUTTLE Robotics)

Part Number: SK-TDA4VM

Hi

I am with SCUTTLE Robotics organization, currently working to get the SK-TDA4VM Edge-Al board up and running on a SCUTTLE bot. I followed this getting started guide to boot up the SK-TDA4VM Edge-Al board successfully. Currently it seems the only way to remotely connect to the board is to ssh into the device using the ip_eth0 shown on the display, or through the IP address of the wireless access point if the Wi-Fi card is installed on the board. I would like to inquire if there is a way to acquire the IP address of the wireless access point without having to connect a display to the board when trying to remotely ssh into the device? 

Kind Regards

Chukwubuikem Ewelike (BK)

SCUTTLE Robotics