This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti's exports,
I have a question about the Lens Distortion Correction (LDC) block. I saw the ldc Supporting up to 8192 x 8192 image dimension. Our image size is 1280*5120.
According to the following instructions,the Bit width of signed integer offset in verical direction or horizontal direction only seems to be 12.
That is, the maximum range that can support pixel translation is [-4096, 4096], am I right?
Is there one way to expand the translation range?
Can the precision be changed from 1/8th pixel to 1 pixel ?