Part Number: AM625
Other Parts Discussed in Thread: TPS3897
Hi,
According to the datasheet of the AM6252, reset timing section, 9500000 ns hold time is required after all supplies valid. But I cannot see any delay part in the reference design schematics. How does the reference design ensure this hold time?
In addition, we do not plan to use the following signals which is used to manage the MCU_PORz in the reference design:
- TEST_PORZn
- VCC_5V0_PG
- JTAG_EMU_RSTn
- SoC_PORz
- CONN_MCU_PORz
Thats why I only want to use 0.85V (VDDR_CORE) regulator power good (PG) output to assert the MCU_PORz signal.
Is it appropriate to directly use just 0.85V PG output for PORz asserting? In that case, should we use RC delay circuit etc. on the MCU_PORz line to provide 9500000 ns hold time?
Thanks for your help in advance.