This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: SK-AM62 EVM does not boot

Part Number: AM625
Other Parts Discussed in Thread: SK-AM62

Hi,

I have a SK-AM62 EVM board, I have followed the all required steps written on the Quick Start Gude but the board does not boot.

I've used WIC image downloaded from this link: "https://dr-download.ti.com/software-development/software-development-kit-sdk/MD-PvdSyIiioq/08.03.00.19/tisdk-default-image-am62xx-evm.wic.xz" and Balena Etcher to prepare a SD card.

Power indication LED's are on, voltage rails are valid, serial ports showing and I selected first port of them but serial port does not promt anything except "-" sign.

What can be the possible cause? How can I fix this? Thanks in advance.

  • Hello,
    I'm attaching the boot log I captured from SD boot using SDK 8.3 on AM62x-SK E1 board for your reference.
    Have we checked the boot mode switch setting (SW2 & SW1) on your board?
    Note that the boot mode orientation (SW2 & SW1) has changed between E1 and E2.
    www.ti.com/.../spruj40
    Best,
    -Hong

    U-Boot SPL 2021.01-g74fc69c889 (May 30 2022 - 16:40:44 +0000)
    SYSFW ABI: 3.1 (firmware rev 0x0008 '8.3.2--v08.03.02 (Jolly Jellyfi')
    Trying to boot from MMC2
    Loading Environment from MMC... *** Warning - No MMC card found, using default environment
    
    Starting ATF on ARM64 core...
    
    NOTICE:  BL31: v2.6(release):08.03.00.003-dirty
    NOTICE:  BL31: Built : 16:35:46, May 30 2022
    
    U-Boot SPL 2021.01-g74fc69c889 (May 30 2022 - 16:39:30 +0000)
    SYSFW ABI: 3.1 (firmware rev 0x0008 '8.3.2--v08.03.02 (Jolly Jellyfi')
    Trying to boot from MMC2
    
    
    U-Boot 2021.01-g74fc69c889 (May 30 2022 - 16:39:30 +0000)
    
    SoC:   AM62X SR1.0
    Model: Texas Instruments AM625 SK
    EEPROM not available at 0x50, trying to read at 0x51
    Board: AM62-SKEVM rev E1
    DRAM:  2 GiB
    MMC:   mmc@fa10000: 0, mmc@fa00000: 1, mmc@fa20000: 2
    Loading Environment from MMC... OK
    In:    serial@2800000
    Out:   serial@2800000
    Err:   serial@2800000
    Net:   eth0: ethernet@8000000port@1
    Hit any key to stop autoboot:  2  0 
    => md.l 0x43000030 1
    43000030: 00000243                               C...
    => 

  • Hi,

    Thanks for your help Hong. I've checked the bootmode switches, it seems correct, could you please also check it. 

  • Hi again,

    It is because of the false boot options as you said, issue is solved, thanks.