Part Number: SK-TDA4VM
Other Parts Discussed in Thread: TDA4VM
Issue : I am unable to read or set a lower resolution on the GStreamer pipeline to read from the Pi v2 Camera
I have a TDA4VM Starter which I want to use for a custom application. I need to read the video stream at a resolution of 640x480. However, If I set it to anything below 1920x1080, it is not able to get the buffer for the frames.
Gstreamer src string: "v4l2src device=/dev/video2 ! queue leaky=2 ! video/x-bayer, width=1920, height=1080, format=rggb, framerate=250/1 ! tiovxisp sink_0::device=/dev/v4l-subdev2 sensor-name=SENSOR_SONY_IMX219_RPI dcc-isp-file=/opt/imaging/imx219/dcc_viss.bin sink_0::dcc-2a-file=/opt/imaging/imx219/dcc_2a.bin format-msb=7 ! video/x-raw, format=NV12 ! tiovxcolorconvert target=0 in-pool-size=4 out-pool-size=4 ! video/x-raw,format=RGB ! appsink name=sen_0 max-buffers=4 drop=true"
I am using the gstreamer wrapper buffer provided with the SDK.
Could someone please help me with this?