Part Number: AM625
The text below is from SPRUIV7 – MAY 2022. Please provide the missing table of ring Accelerator mapping indicated below, or confirm that the mapping ranges do not apply to the AM625
------
11.2.1.3.1.1 DMSS Interrupt Description
This section describes the interrupt-related information that flows within DMSS and how this information is
configured or generated.
1. Ring Number (R#)
• Data is read from and written to a specific Ring Accelerator ring using direct ring-mode, or secure proxy
access
• The Ring Accelerator has specific ring number ranges for specific purposes. The R# must match
the intended purpose of the ring (see Table 10-578, RINGACC Ring Mapping) <Section under
development: no ring mapping section in spec, need to confirm if it exists in a different place
or just discard this sentence>