Part Number: TMS320C6713B
Device specifics:
TMS32057C13BGDP
C20-19A86KW
1527332
We have uncovered CCAs with TMS320C6713B DSPs that fail to properly assert CE1 at cold temperature which causes the EMIF Boot mode to fail. When this occurs, the 1K ROM image DMA-transfer to internal SRAM is incomplete or is partial causing the DSP to go off into space when executed: the DSP won’t recover unless the power is reset at a higher temperature. We’ve noted at least eight CCAs that fail this way in the last year or so, likely more.
During power resets at low temperature the EMIF Chip Enables are not asserting correctly; either partially, sporadically, or not at all. The DSP is hardware wired for EMIF boot using default ROM timings or which the boot EDMA transfers the first 1KB from flash on CE 1 to internal SRAM for execution. When CE 1 fails to assert correctly, the flash content is read as garbage which causes the DSP to go off into the weeds when executed. The DSP starts to recover above approximately -30OC with a power reset ( without a reset the DSP will never recover ).
Are there any known issues with the TI DSP TMS320 6713B EMIF Chip Enables (CE 0,1,2,3) below -30C?
Mike