Part Number: 66AK2G12
Other Parts Discussed in Thread: 66AK2H06
Hi,
I have questions from my customer for 66AK2G12 PCIe SERDES configuration.
According to below document section 2.3, there are three SERDES types.
https://www.ti.com/jp/lit/ug/spruho3a/spruho3a.pdf
PHY-A 2 Lane
PHY-A 4 Lane
PHY-B
But 66AK2G12 has only 1 Lane (Lane0 TX0, RX0).
And the section 2.2 in the same document says, customer needs to use TI generated default PHY configuration in MCSDK.
MCSDK configured all four lanes (address 0x02320400-, 0x02320600-, and 0x02320800-).
These three lanes can be left untouched?
Could you provide sample code for PCIe configuration?
Customer refers to below code from
\ti\pdk_keystone2_3_00_03_15\packages\ti\drv\pcie\example\sample\src\pcie_sample.c
But it seems old one and this is for 66AK2H06.
/* ============================================================================
* Copyright (c) Texas Instruments Incorporated 2010-2013
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/**
* @file pcie_sample.c
*
* @brief
* This is the PCIe example code.
*
*/
/**
* In the PCIe sample example two Shannon EVMs are used to test the PCIe driver.
* As described in the following figure, Shannon 1 is configured as a Root Complex
* and Shannon 2 is configured as End Point.
*
* Shannon 1 Shannon 2
* ------------------ -------------------
* | | | |
* | Root | PCIe Link | End Point |
* | Complex | <-------------------------->| |
* | | | |
* ------------------ -------------------
*
* Once the PCIe link is established, the following sequence of actions will happen:
* - Shannon 1 sends data to Shannon 2
* - Shannon 2 waits to receive all the data
* - Shannon 2 sends the data back to Shannon 1
* - Shannon 1 waits to receive all the data
* - Shannon 1 verifies if the received data matches the sent data and declares test pass or fail.
*
*/
#include "pcie_sample.h"
#include <ti/drv/pcie/device/pcie_device.h>
/* Use regular "printf" when not using BIOS */
//#include <xdc/runtime/System.h>
#define System_printf printf
#include <stdio.h>
#include <ti/csl/csl_bootcfgAux.h>
#include <ti/csl/csl_cacheAux.h>
#include <ti/csl/csl_chip.h>
#include <ti/csl/csl_xmcAux.h>
#pragma DATA_SECTION(dstBuf, ".dstBufSec")
/* Cache coherence: Align must be a multiple of cache line size (L2=128 bytes, L1=64 bytes) to operate with cache enabled. */
/* Aligning to 256 bytes because the PCIe inbound offset register masks the last 8bits of the buffer address */
#pragma DATA_ALIGN(dstBuf, 256)
/* last element in the buffer is a marker that indicates the buffer status: full/empty */
#define PCIE_EXAMPLE_MAX_CACHE_LINE_SIZE 128
#define PCIE_EXAMPLE_UINT32_SIZE 4 /* preprocessor #if requires a real constant, not a sizeof() */
#define PCIE_EXAMPLE_DSTBUF_BYTES ((PCIE_BUFSIZE_APP + 1) * PCIE_EXAMPLE_UINT32_SIZE)
#define PCIE_EXAMPLE_DSTBUF_REM (PCIE_EXAMPLE_DSTBUF_BYTES % PCIE_EXAMPLE_MAX_CACHE_LINE_SIZE)
#define PCIE_EXAMPLE_DSTBUF_PAD (PCIE_EXAMPLE_DSTBUF_REM ? (PCIE_EXAMPLE_MAX_CACHE_LINE_SIZE - PCIE_EXAMPLE_DSTBUF_REM) : 0)
struct dstBuf_s {
volatile uint32_t buf[PCIE_BUFSIZE_APP + 1];
/* Cache coherence: Must pad to cache line size in order to enable cacheability */
#if PCIE_EXAMPLE_DSTBUF_PAD
uint8_t padding[PCIE_EXAMPLE_DSTBUF_PAD];
#endif
} dstBuf;
#define PCIE_EXAMPLE_BUF_EMPTY 0
#define PCIE_EXAMPLE_BUF_FULL 1
/* Does not need to be aligned (even for cache) since it is only accessed locally */
uint32_t srcBuf[PCIE_BUFSIZE_APP];
extern volatile unsigned int cregister TSCL;
/* Global config variable that controls
the PCIe mode. It is global so it can be poked
from CCS. It should be set either to EP or RC. */
pcieMode_e PcieModeGbl = pcie_EP_MODE;
#if defined(DEVICE_K2K) || defined(DEVICE_K2H)
/**********************************************************************************
* FUNCTION PURPOSE: Function for updating register value with mask
**********************************************************************************
* DESCRIPTION: Function for updating register value with mask
**********************************************************************************/
static void write_32_mask(volatile uint32_t base_addr,
uint32_t offset,
uint32_t mask,
uint32_t write_data)
{
uint32_t read_data, data;
read_data = (*(volatile uint32_t *)(base_addr + offset));
data = (write_data & ~mask ) | (read_data & mask);
(*(uint32_t *) ((base_addr + offset))) = data;
}
void reg_poll(volatile unsigned int addr, volatile unsigned int poll_val, volatile unsigned int masked_bits)
{
volatile unsigned int read_data;
read_data = (*(unsigned int *) (addr));
read_data = read_data & masked_bits;
while (read_data != (poll_val & masked_bits))
{
read_data = (*(unsigned int *) (addr));
read_data = read_data & masked_bits;
}
}
void pcieSSDefSbSerdesSetup(volatile uint32_t base_addr)
{
write_32_mask(base_addr, 0x000,0xffff00ff,0x00000800);
write_32_mask(base_addr, 0x0060,0xff000000,0x00041c5c);
write_32_mask(base_addr, 0x0064,0x000000ff,0x0343c700);
write_32_mask(base_addr, 0x006c,0xffffff00,0x00000012);
write_32_mask(base_addr, 0x0068,0xff00ffff,0x00070000);
write_32_mask(base_addr, 0x0078,0xffff00ff,0x0000c000);
write_32_mask(base_addr, 0x0200,0xffffff00,0x00000000);
write_32_mask(base_addr, 0x0204,0x00ffff00,0x5e000080);
write_32_mask(base_addr, 0x0208,0xffffff00,0x00000006);
write_32_mask(base_addr, 0x0210,0xffffff00,0x00000023);
write_32_mask(base_addr, 0x0214,0x00ff0000,0x2e003060);
write_32_mask(base_addr, 0x0218,0x00ffffff,0x76000000);
write_32_mask(base_addr, 0x022c,0xff00ff00,0x00100002);
write_32_mask(base_addr, 0x02a0,0x0000ffff,0xffee0000);
write_32_mask(base_addr, 0x02a4,0xffffff00,0x0000000f);
write_32_mask(base_addr, 0x0204,0x00ffffff,0x5e000000);
write_32_mask(base_addr, 0x0208,0xffffff00,0x00000006);
write_32_mask(base_addr, 0x0278,0xffff00ff,0x00002000);
write_32_mask(base_addr, 0x0280,0xff00ff00,0x00280028);
write_32_mask(base_addr, 0x0284,0x00000000,0x2d0f0385);
write_32_mask(base_addr, 0x0250,0x00ffffff,0xd0000000);
write_32_mask(base_addr, 0x0284,0xffffff00,0x00000085);
write_32_mask(base_addr, 0x0294,0x00ffffff,0x20000000);
write_32_mask(base_addr, 0x0400,0xffffff00,0x00000000);
write_32_mask(base_addr, 0x0404,0x00ffff00,0x5e000080);
write_32_mask(base_addr, 0x0408,0xffffff00,0x00000006);
write_32_mask(base_addr, 0x0410,0xffffff00,0x00000023);
write_32_mask(base_addr, 0x0414,0x00ff0000,0x2e003060);
write_32_mask(base_addr, 0x0418,0x00ffffff,0x76000000);
write_32_mask(base_addr, 0x042c,0xff00ff00,0x00100002);
write_32_mask(base_addr, 0x04a0,0x0000ffff,0xffee0000);
write_32_mask(base_addr, 0x04a4,0xffffff00,0x0000000f);
write_32_mask(base_addr, 0x0404,0x00ffffff,0x5e000000);
write_32_mask(base_addr, 0x0408,0xffffff00,0x00000006);
write_32_mask(base_addr, 0x0478,0xffff00ff,0x00002000);
write_32_mask(base_addr, 0x0480,0xff00ff00,0x00280028);
write_32_mask(base_addr, 0x0484,0x00000000,0x2d0f0385);
write_32_mask(base_addr, 0x0450,0x00ffffff,0xd0000000);
write_32_mask(base_addr, 0x0494,0x00ffffff,0x20000000);
write_32_mask(base_addr, 0x0604,0xffffff00,0x00000080);
write_32_mask(base_addr, 0x0600,0xffffff00,0x00000000);
write_32_mask(base_addr, 0x0604,0x00ffffff,0x5e000000);
write_32_mask(base_addr, 0x0608,0xffffff00,0x00000006);
write_32_mask(base_addr, 0x0610,0xffffff00,0x00000023);
write_32_mask(base_addr, 0x0614,0x00ff0000,0x2e003060);
write_32_mask(base_addr, 0x0618,0x00ffffff,0x76000000);
write_32_mask(base_addr, 0x062c,0xff00ff00,0x00100002);
write_32_mask(base_addr, 0x06a0,0x0000ffff,0xffee0000);
write_32_mask(base_addr, 0x06a4,0xffffff00,0x0000000f);
write_32_mask(base_addr, 0x0604,0x00ffffff,0x5e000000);
write_32_mask(base_addr, 0x0608,0xffffff00,0x00000006);
write_32_mask(base_addr, 0x0678,0xffff00ff,0x00002000);
write_32_mask(base_addr, 0x0680,0xff00ff00,0x00280028);
write_32_mask(base_addr, 0x0684,0x00000000,0x2d0f0385);
write_32_mask(base_addr, 0x0650,0x00ffffff,0xd0000000);
write_32_mask(base_addr, 0x0694,0x00ffffff,0x20000000);
write_32_mask(base_addr, 0x0800,0xffffff00,0x00000000);
write_32_mask(base_addr, 0x0804,0x00ffff00,0x5e000080);
write_32_mask(base_addr, 0x0808,0xffffff00,0x00000006);
write_32_mask(base_addr, 0x0810,0xffffff00,0x00000023);
write_32_mask(base_addr, 0x0814,0x00ff0000,0x2e003060);
write_32_mask(base_addr, 0x0818,0x00ffffff,0x76000000);
write_32_mask(base_addr, 0x082c,0xff00ff00,0x00100002);
write_32_mask(base_addr, 0x08a0,0x0000ffff,0xffee0000);
write_32_mask(base_addr, 0x08a4,0xffffff00,0x0000000f);
write_32_mask(base_addr, 0x0804,0x00ffffff,0x5e000000);
write_32_mask(base_addr, 0x0808,0xffffff00,0x00000006);
write_32_mask(base_addr, 0x0878,0xffff00ff,0x00002000);
write_32_mask(base_addr, 0x0880,0xff00ff00,0x00280028);
write_32_mask(base_addr, 0x0884,0x00000000,0x2d0f0385);
write_32_mask(base_addr, 0x0850,0x00ffffff,0xd0000000);
write_32_mask(base_addr, 0x0894,0x00ffffff,0x20000000);
write_32_mask(base_addr, 0x0a00,0xffff00ff,0x00000100);
write_32_mask(base_addr, 0x0a08,0xff000000,0x00e12c08);
write_32_mask(base_addr, 0x0a0c,0xffffff00,0x00000081);
write_32_mask(base_addr, 0x0a18,0xff00ffff,0x00e80000);
write_32_mask(base_addr, 0x0a30,0x00ffff00,0x002f2f00);
write_32_mask(base_addr, 0x0a48,0xff0000ff,0x00e3ce00);
write_32_mask(base_addr, 0x0a4c,0x0000ffff,0xac820000);
write_32_mask(base_addr, 0x0a54,0x00ffffff,0xc0000000);
write_32_mask(base_addr, 0x0a58,0xffff0000,0x00001441);
write_32_mask(base_addr, 0x0a84,0xffff0000,0x00000301);
write_32_mask(base_addr, 0x0a8c,0x0000ffff,0x81030000);
write_32_mask(base_addr, 0x0a90,0xffff0000,0x00006001);
write_32_mask(base_addr, 0x0a94,0x00ffffff,0x01000000);
write_32_mask(base_addr, 0x0aa0,0x00ffffff,0x81000000);
write_32_mask(base_addr, 0x0abc,0x00ffffff,0xff000000);
write_32_mask(base_addr, 0x0ac0,0xffffff00,0x0000008b);
write_32_mask(base_addr, 0x0000,0xffffff00,0x00000003);
write_32_mask(base_addr, 0x0a00,0xffffff00,0x0000009f);
}
#endif
/*****************************************************************************
* Function: Power domain configuration
****************************************************************************/
pcieRet_e pciePowerCfg(void)
{
/* Turn on the PCIe power domain */
if (CSL_PSC_getPowerDomainState (CSL_PSC_PD_PCIE) != PSC_PDSTATE_ON) {
/* Enable the domain */
CSL_PSC_enablePowerDomain (CSL_PSC_PD_PCIE);
/* Enable MDCTL */
CSL_PSC_setModuleNextState (CSL_PSC_LPSC_PCIE, PSC_MODSTATE_ENABLE);
/* Apply the domain */
CSL_PSC_startStateTransition (CSL_PSC_PD_PCIE);
/* Wait for it to finish */
while (! CSL_PSC_isStateTransitionDone (CSL_PSC_PD_PCIE));
} else {
System_printf ("Power domain is already enabled. You probably re-ran without device reset (which is OK)\n");
}
return pcie_RET_OK;
}
/*****************************************************************************
* Function: Utility function to introduce delay
****************************************************************************/
void cycleDelay (uint32_t count)
{
uint32_t sat;
if (count <= 0)
return;
sat = TSCL + count;
while (TSCL < sat);
}
/*****************************************************************************
* Function: Serdes configuration
****************************************************************************/
pcieRet_e pcieSerdesCfg(void)
{
#if !defined(DEVICE_K2K) && !defined(DEVICE_K2H)
uint16_t cfg;
#endif
#if !defined(DEVICE_K2K) && !defined(DEVICE_K2H)
/* Provide PLL reference clock to SERDES inside PCIESS
Program PLL settings and enable PLL from PCIe SERDES.*/
cfg = 0x01C9; /* value based on PCIe userguide */
CSL_BootCfgSetPCIEConfigPLL(cfg);
#else /* !DEVICE_K2K && !DEVICE_K2H */
#ifndef SIMULATOR_SUPPORT
//CSL_PciessDefSbSerdesSetup();
pcieSSDefSbSerdesSetup(CSL_PCIE_SERDES_CFG_REGS);
#endif
#endif
/*Wait for PLL to lock (3000 CLKIN1 cycles) */
cycleDelay(10000);
return pcie_RET_OK;
}
/*****************************************************************************
* Function: Enable/Disable LTSSM (Link Training)
****************************************************************************/
pcieRet_e pcieLtssmCtrl(Pcie_Handle handle, uint8_t enable)
{
pcieCmdStatusReg_t cmdStatus;
pcieRegisters_t setRegs;
pcieRegisters_t getRegs;
pcieRet_e retVal;
memset (&cmdStatus, 0, sizeof(cmdStatus));
memset (&setRegs, 0, sizeof(setRegs));
memset (&getRegs, 0, sizeof(getRegs));
getRegs.cmdStatus = &cmdStatus;
if ((retVal = Pcie_readRegs (handle, pcie_LOCATION_LOCAL, &getRegs)) != pcie_RET_OK)
{
System_printf ("Read CMD STATUS register failed!\n");
return retVal;
}
if(enable)
cmdStatus.ltssmEn = 1;
else
cmdStatus.ltssmEn = 0;
setRegs.cmdStatus = &cmdStatus;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET CMD STATUS register failed!\n");
return retVal;
}
return pcie_RET_OK;
}
/*****************************************************************************
* Function: Configure PCIe in Root Complex Mode
****************************************************************************/
pcieRet_e pcieCfgRC(Pcie_Handle handle)
{
pcieRet_e retVal;
pcieCmdStatusReg_t cmdStatus;
pcieObSizeReg_t obSize;
pcieGen2Reg_t gen2;
pcieType1Bar32bitIdx_t type1Bar32bitIdx;
pcieStatusCmdReg_t statusCmd;
pcieDevStatCtrlReg_t devStatCtrl;
pcieAccrReg_t accr;
pcieRegisters_t setRegs;
pcieRegisters_t getRegs;
memset (&cmdStatus, 0, sizeof(cmdStatus));
memset (&obSize, 0, sizeof(obSize));
memset (&gen2, 0, sizeof(gen2));
memset (&type1Bar32bitIdx, 0, sizeof(type1Bar32bitIdx));
memset (&statusCmd, 0, sizeof(statusCmd));
memset (&devStatCtrl, 0, sizeof(devStatCtrl));
memset (&accr, 0, sizeof(accr));
/*Disable link training*/
if ((retVal = pcieLtssmCtrl(handle, FALSE)) != pcie_RET_OK)
{
System_printf ("Failed to disable Link Training!\n");
return retVal;
}
/* Configure the size of the translation regions */
memset (&setRegs, 0, sizeof(setRegs));
memset (&getRegs, 0, sizeof(getRegs));
obSize.size = pcie_OB_SIZE_8MB;
setRegs.obSize = &obSize;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET OB_SIZE register failed!\n");
return retVal;
}
/* Setting PL_GEN2 */
memset (&setRegs, 0, sizeof(setRegs));
gen2.numFts = 0xF;
gen2.dirSpd = 0x0;
gen2.lnEn = 1;
setRegs.gen2 = &gen2;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET GEN2 register failed!\n");
return retVal;
}
/* Configure BAR Masks */
/* First need to enable writing on BAR mask registers */
memset (&setRegs, 0, sizeof(setRegs));
memset (&getRegs, 0, sizeof(getRegs));
memset (&cmdStatus, 0, sizeof(cmdStatus));
getRegs.cmdStatus = &cmdStatus;
if ((retVal = Pcie_readRegs (handle, pcie_LOCATION_LOCAL, &getRegs)) != pcie_RET_OK)
{
System_printf ("Read CMD STATUS register failed!\n");
return retVal;
}
cmdStatus.dbi = 1;
setRegs.cmdStatus = &cmdStatus;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET CMD STATUS register failed!\n");
return retVal;
}
/* Configure Masks*/
memset (&setRegs, 0, sizeof(setRegs));
type1Bar32bitIdx.reg.reg32 = PCIE_BAR_MASK;
setRegs.type1Bar32bitIdx = &type1Bar32bitIdx;
/* BAR 0 */
type1Bar32bitIdx.idx = 0; /* configure BAR 0*/
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET BAR MASK register failed!\n");
return retVal;
}
/* BAR 1 */
type1Bar32bitIdx.idx = 1; /* configure BAR 1*/
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET BAR MASK register failed!\n");
return retVal;
}
/* Disable writing on BAR Masks */
memset (&setRegs, 0, sizeof(setRegs));
memset (&getRegs, 0, sizeof(getRegs));
memset (&cmdStatus, 0, sizeof(cmdStatus));
getRegs.cmdStatus = &cmdStatus;
if ((retVal = Pcie_readRegs (handle, pcie_LOCATION_LOCAL, &getRegs)) != pcie_RET_OK)
{
System_printf ("Read CMD STATUS register failed!\n");
return retVal;
}
cmdStatus.dbi = 0;
setRegs.cmdStatus = &cmdStatus;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET CMD STATUS register failed!\n");
return retVal;
}
/* Enable memory access and mastership of the bus */
memset (&setRegs, 0, sizeof(setRegs));
memset (&getRegs, 0, sizeof(getRegs));
getRegs.statusCmd = &statusCmd;
if ((retVal = Pcie_readRegs (handle, pcie_LOCATION_LOCAL, &getRegs)) != pcie_RET_OK)
{
System_printf ("Read Status Comand register failed!\n");
return retVal;
}
statusCmd.memSp = 1;
statusCmd.busMs = 1;
statusCmd.resp = 1;
statusCmd.serrEn = 1;
setRegs.statusCmd = &statusCmd;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET Status Command register failed!\n");
return retVal;
}
/* Enable Error Reporting */
memset (&setRegs, 0, sizeof(setRegs));
memset (&getRegs, 0, sizeof(getRegs));
getRegs.devStatCtrl = &devStatCtrl;
if ((retVal = Pcie_readRegs (handle, pcie_LOCATION_LOCAL, &getRegs)) != pcie_RET_OK)
{
System_printf ("Regad Device Status Control register failed!\n");
return retVal;
}
devStatCtrl.reqRp = 1;
devStatCtrl.fatalErRp = 1;
devStatCtrl.nFatalErRp = 1;
devStatCtrl.corErRp = 1;
setRegs.devStatCtrl = &devStatCtrl;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET Device Status Control register failed!\n");
return retVal;
}
/* Enable ECRC */
memset (&setRegs, 0, sizeof(setRegs));
accr.chkEn=1;
accr.chkCap=1;
accr.genEn=1;
accr.genCap=1;
setRegs.accr = &accr;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET ACCR register failed!\n");
return retVal;
}
return pcie_RET_OK;
}
/*****************************************************************************
* Function: Configure PCIe in End Point Mode
****************************************************************************/
pcieRet_e pcieCfgEP(Pcie_Handle handle)
{
pcieRet_e retVal;
pcieCmdStatusReg_t cmdStatus;
pcieObSizeReg_t obSize;
pcieGen2Reg_t gen2;
pcieType0Bar32bitIdx_t type0Bar32bitIdx;
pcieStatusCmdReg_t statusCmd;
pcieDevStatCtrlReg_t devStatCtrl;
pcieAccrReg_t accr;
pcieRegisters_t setRegs;
pcieRegisters_t getRegs;
memset (&cmdStatus, 0, sizeof(cmdStatus));
memset (&obSize, 0, sizeof(obSize));
memset (&gen2, 0, sizeof(gen2));
memset (&type0Bar32bitIdx, 0, sizeof(type0Bar32bitIdx));
memset (&statusCmd, 0, sizeof(statusCmd));
memset (&devStatCtrl, 0, sizeof(devStatCtrl));
memset (&accr, 0, sizeof(accr));
/*Disable link training*/
if ((retVal = pcieLtssmCtrl(handle, FALSE)) != pcie_RET_OK)
{
System_printf ("Failed to disable Link Training!\n");
return retVal;
}
/* Configure the size of the translation regions */
memset (&setRegs, 0, sizeof(setRegs));
memset (&getRegs, 0, sizeof(getRegs));
obSize.size = pcie_OB_SIZE_8MB;
setRegs.obSize = &obSize;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET OB_SIZE register failed!\n");
return retVal;
}
/* Setting PL_GEN2 */
memset (&setRegs, 0, sizeof(setRegs));
gen2.numFts = 0xF;
gen2.dirSpd = 0x0;
gen2.lnEn = 1;
setRegs.gen2 = &gen2;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET GEN2 register failed!\n");
return retVal;
}
/* Configure BAR Masks */
/* First need to enable writing on BAR mask registers */
memset (&setRegs, 0, sizeof(setRegs));
memset (&getRegs, 0, sizeof(getRegs));
memset (&cmdStatus, 0, sizeof(cmdStatus));
getRegs.cmdStatus = &cmdStatus;
if ((retVal = Pcie_readRegs (handle, pcie_LOCATION_LOCAL, &getRegs)) != pcie_RET_OK)
{
System_printf ("Read CMD STATUS register failed!\n");
return retVal;
}
cmdStatus.dbi = 1;
setRegs.cmdStatus = &cmdStatus;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET CMD STATUS register failed!\n");
return retVal;
}
/* Configure Masks*/
memset (&setRegs, 0, sizeof(setRegs));
type0Bar32bitIdx.reg.reg32 = PCIE_BAR_MASK;
setRegs.type0Bar32bitIdx = &type0Bar32bitIdx;
/* BAR 0 */
type0Bar32bitIdx.idx = 0; /* configure BAR 0*/
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET BAR MASK register failed!\n");
return retVal;
}
/* BAR 1 */
type0Bar32bitIdx.idx = 1; /* configure BAR 1*/
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET BAR MASK register failed!\n");
return retVal;
}
/* Disable writing on BAR Masks */
memset (&setRegs, 0, sizeof(setRegs));
memset (&getRegs, 0, sizeof(getRegs));
memset (&cmdStatus, 0, sizeof(cmdStatus));
getRegs.cmdStatus = &cmdStatus;
if ((retVal = Pcie_readRegs (handle, pcie_LOCATION_LOCAL, &getRegs)) != pcie_RET_OK)
{
System_printf ("Read CMD STATUS register failed!\n");
return retVal;
}
cmdStatus.dbi = 0;
setRegs.cmdStatus = &cmdStatus;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET CMD STATUS register failed!\n");
return retVal;
}
/* Enable memory access and mastership of the bus */
memset (&setRegs, 0, sizeof(setRegs));
memset (&getRegs, 0, sizeof(getRegs));
getRegs.statusCmd = &statusCmd;
if ((retVal = Pcie_readRegs (handle, pcie_LOCATION_LOCAL, &getRegs)) != pcie_RET_OK)
{
System_printf ("Read Status Comand register failed!\n");
return retVal;
}
statusCmd.memSp = 1;
statusCmd.busMs = 1;
statusCmd.resp = 1;
statusCmd.serrEn = 1;
setRegs.statusCmd = &statusCmd;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET Status Command register failed!\n");
return retVal;
}
/* Enable Error Reporting */
memset (&setRegs, 0, sizeof(setRegs));
memset (&getRegs, 0, sizeof(getRegs));
getRegs.devStatCtrl = &devStatCtrl;
if ((retVal = Pcie_readRegs (handle, pcie_LOCATION_LOCAL, &getRegs)) != pcie_RET_OK)
{
System_printf ("Regad Device Status Control register failed!\n");
return retVal;
}
devStatCtrl.reqRp = 1;
devStatCtrl.fatalErRp = 1;
devStatCtrl.nFatalErRp = 1;
devStatCtrl.corErRp = 1;
setRegs.devStatCtrl = &devStatCtrl;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET Device Status Control register failed!\n");
return retVal;
}
/* Enable ECRC */
memset (&setRegs, 0, sizeof(setRegs));
accr.chkEn=1;
accr.chkCap=1;
accr.genEn=1;
accr.genCap=1;
setRegs.accr = &accr;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET ACCR register failed!\n");
return retVal;
}
return pcie_RET_OK;
}
/*****************************************************************************
* Function: Configure and enable Outbound Address Translation
****************************************************************************/
pcieRet_e pcieObTransCfg(Pcie_Handle handle, uint32_t obAddrLo, uint32_t obAddrHi, uint8_t region)
{
pcieRet_e retVal;
pcieRegisters_t setRegs;
pcieRegisters_t getRegs;
pcieCmdStatusReg_t cmdStatus;
memset (&setRegs, 0, sizeof(setRegs));
memset (&getRegs, 0, sizeof(getRegs));
memset (&cmdStatus, 0, sizeof(cmdStatus));
/* Set outbound offset registers */
if ((retVal = Pcie_cfgObOffset(handle, obAddrLo, obAddrHi, region)) != pcie_RET_OK)
{
System_printf ("Failed to configure ObOffset registers!\n");
return retVal;
}
/*enable Outbound address translation*/
memset (&setRegs, 0, sizeof(setRegs));
memset (&getRegs, 0, sizeof(getRegs));
getRegs.cmdStatus = &cmdStatus;
if ((retVal = Pcie_readRegs (handle, pcie_LOCATION_LOCAL, &getRegs)) != pcie_RET_OK)
{
System_printf ("Read CMD STATUS register failed!\n");
return retVal;
}
cmdStatus.obXltEn = 1;
setRegs.cmdStatus = &cmdStatus;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET CMD STATUS register failed!\n");
return retVal;
}
return pcie_RET_OK;
}
/*****************************************************************************
* Function: Configure and enable Inbound Address Translation
****************************************************************************/
pcieRet_e pcieIbTransCfg(Pcie_Handle handle, pcieIbTransCfg_t *ibCfg)
{
pcieRet_e retVal;
pcieRegisters_t setRegs;
pcieRegisters_t getRegs;
pcieCmdStatusReg_t cmdStatus;
memset (&setRegs, 0, sizeof(setRegs));
memset (&getRegs, 0, sizeof(getRegs));
memset (&cmdStatus, 0, sizeof(cmdStatus));
/* Set outbound offset registers */
if ((retVal = Pcie_cfgIbTrans(handle, ibCfg)) != pcie_RET_OK)
{
System_printf ("Failed to configure Inbound Translation registers!\n");
return retVal;
}
/*enable Inbound address translation*/
memset (&setRegs, 0, sizeof(setRegs));
memset (&getRegs, 0, sizeof(getRegs));
getRegs.cmdStatus = &cmdStatus;
if ((retVal = Pcie_readRegs (handle, pcie_LOCATION_LOCAL, &getRegs)) != pcie_RET_OK)
{
System_printf ("Read CMD STATUS register failed!\n");
return retVal;
}
cmdStatus.ibXltEn = 1;
setRegs.cmdStatus = &cmdStatus;
if ((retVal = Pcie_writeRegs (handle, pcie_LOCATION_LOCAL, &setRegs)) != pcie_RET_OK)
{
System_printf ("SET CMD STATUS register failed!\n");
return retVal;
}
return pcie_RET_OK;
}
/*****************************************************************************
* Function: Initialize application buffers
****************************************************************************/
void pcieInitAppBuf(void)
{
uint32_t i;
for (i=0; i<PCIE_BUFSIZE_APP; i++)
{
dstBuf.buf[i] = 0;
srcBuf[i] = i;
}
dstBuf.buf[PCIE_BUFSIZE_APP] = PCIE_EXAMPLE_BUF_EMPTY;
}
/*****************************************************************************
* Function: Check LTSSM status and wait for the link to be up
****************************************************************************/
void pcieWaitLinkUp(Pcie_Handle handle)
{
pcieRegisters_t getRegs;
pcieDebug0Reg_t debug0;
memset (&debug0, 0, sizeof(debug0));
memset (&getRegs, 0, sizeof(getRegs));
uint8_t ltssmState = 0;
while(ltssmState != pcie_LTSSM_L0)
{
cycleDelay(100);
getRegs.debug0 = &debug0;
if (Pcie_readRegs (handle, pcie_LOCATION_LOCAL, &getRegs) != pcie_RET_OK)
{
System_printf ("Read LTSSM state failed!\n");
return;
}
ltssmState = debug0.ltssmState;
}
}
/*****************************************************************************
* Function: Converts a core local L2 address to a global L2 address
* Input addr: L2 address to be converted to global.
* return: uint32_t Global L2 address
*****************************************************************************/
uint32_t pcieConvert_CoreLocal2GlobalAddr (uint32_t addr)
{
uint32_t coreNum;
/* Get the core number. */
coreNum = CSL_chipReadReg(CSL_CHIP_DNUM);
/* Compute the global address. */
return ((1 << 28) | (coreNum << 24) | (addr & 0x00ffffff));
}
/*****************************************************************************
* Function: Main
****************************************************************************/
void main (void)
{
TSCL = 1;
#if !defined(DEVICE_K2K) && !defined(DEVICE_K2H)
uint16_t lock=0;
#endif
pcieRet_e retVal;
pcieIbTransCfg_t ibCfg;
pcieBarCfg_t barCfg;
Pcie_Handle handle = NULL;
void *pcieBase;
uint32_t i;
/* Unlock kicker once, and don't relock, because its not multicore safe */
CSL_BootCfgUnlockKicker();
System_printf ("**********************************************\n");
System_printf ("* PCIe Test Start *\n");
if(PcieModeGbl == pcie_RC_MODE)
System_printf ("* RC mode *\n");
else
System_printf ("* EP mode *\n");
System_printf ("**********************************************\n\n");
System_printf ("Version #: 0x%08x; string %s\n\n", Pcie_getVersion(), Pcie_getVersionStr());
/* Pass device config to LLD */
if ((retVal = Pcie_init (&pcieInitCfg)) != pcie_RET_OK)
{
System_printf ("LLD device configuration failed\n");
exit(1);
}
/* Initialize application buffers */
pcieInitAppBuf();
/* Configure SERDES*/
if ((retVal = pcieSerdesCfg()) != pcie_RET_OK) {
System_printf ("PCIe Serdes config failed (%d)\n", (int)retVal);
exit(1);
}
/* Set the PCIe mode*/
if ((retVal = Pcie_setMode(PcieModeGbl)) != pcie_RET_OK) {
System_printf ("Set PCIe Mode failed (%d)\n", (int)retVal);
exit(1);
}
/* Power up PCIe Module */
if ((retVal = pciePowerCfg()) != pcie_RET_OK) {
System_printf ("PCIe Power Up failed (%d)\n", (int)retVal);
exit(1);
}
System_printf ("PCIe Power Up.\n");
/* Wait until the PCIe SERDES PLL locks */
#if !defined(DEVICE_K2K) && !defined(DEVICE_K2H)
while (!lock)
{
CSL_BootCfgGetPCIEPLLLock(&lock);
}
#endif /* !DEVICE_K2K && !DEVICE_K2H */
if ((retVal = Pcie_open(0, &handle)) != pcie_RET_OK)
{
System_printf ("Open failed (%d)\n", (int)retVal);
exit(1);
}
System_printf ("PLL configured.\n");
if(PcieModeGbl == pcie_RC_MODE)
{
/* Configure application registers for Root Complex*/
if ((retVal = pcieCfgRC(handle)) != pcie_RET_OK)
{
System_printf ("Failed to configure PCIe in RC mode (%d)\n", (int)retVal);
exit(1);
}
/* Configure Address Translation */
barCfg.location = pcie_LOCATION_LOCAL;
barCfg.mode = pcie_RC_MODE;
barCfg.base = PCIE_IB_LO_ADDR_M;
barCfg.prefetch = pcie_BAR_NON_PREF;
barCfg.type = pcie_BAR_TYPE32;
barCfg.memSpace = pcie_BAR_MEM_MEM;
barCfg.idx = PCIE_BAR_IDX_M;
if ((retVal = Pcie_cfgBar(handle, &barCfg)) != pcie_RET_OK)
{
System_printf ("Failed to configure BAR (%d)\n", (int)retVal);
exit(1);
}
ibCfg.ibBar = PCIE_BAR_IDX_M; /* Match BAR that was configured above*/
ibCfg.ibStartAddrLo = PCIE_IB_LO_ADDR_M;
ibCfg.ibStartAddrHi = PCIE_IB_HI_ADDR_M;
ibCfg.ibOffsetAddr = (uint32_t)pcieConvert_CoreLocal2GlobalAddr ((uint32_t)dstBuf.buf);
ibCfg.region = PCIE_IB_REGION_M;
if ((retVal = pcieIbTransCfg(handle, &ibCfg)) != pcie_RET_OK)
{
System_printf ("Failed to configure Inbound Translation (%d)\n", (int)retVal);
exit(1);
}
else
{
System_printf ("Successfully configured Inbound Translation!\n");
}
if ((retVal = pcieObTransCfg (handle, PCIE_OB_LO_ADDR_M, PCIE_OB_HI_ADDR_M, PCIE_OB_REGION_M)) != pcie_RET_OK)
{
System_printf ("Failed to configure Outbound Address Translation (%d)\n", (int)retVal);
exit(1);
}
else
{
System_printf ("Successfully configured Outbound Translation!\n");
}
}
else
{
/* Configure application registers for End Point*/
if ((retVal = pcieCfgEP(handle)) != pcie_RET_OK)
{
System_printf ("Failed to configure PCIe in EP mode (%d)\n", (int)retVal);
exit(1);
}
/* Configure Address Translation */
barCfg.location = pcie_LOCATION_LOCAL;
barCfg.mode = pcie_EP_MODE;
barCfg.base = PCIE_IB_LO_ADDR_S;
barCfg.prefetch = pcie_BAR_NON_PREF;
barCfg.type = pcie_BAR_TYPE32;
barCfg.memSpace = pcie_BAR_MEM_MEM;
barCfg.idx = PCIE_BAR_IDX_S;
if ((retVal = Pcie_cfgBar(handle, &barCfg)) != pcie_RET_OK)
{
System_printf ("Failed to configure BAR!\n");
exit(1);
}
ibCfg.ibBar = PCIE_BAR_IDX_S; /* Match BAR that was configured above*/
ibCfg.ibStartAddrLo = PCIE_IB_LO_ADDR_S;
ibCfg.ibStartAddrHi = PCIE_IB_HI_ADDR_S;
ibCfg.ibOffsetAddr = (uint32_t)pcieConvert_CoreLocal2GlobalAddr ((uint32_t)dstBuf.buf);
ibCfg.region = PCIE_IB_REGION_S;
if ((retVal = pcieIbTransCfg(handle, &ibCfg)) != pcie_RET_OK)
{
System_printf ("Failed to configure Inbound Translation!\n", (int)retVal);
exit(1);
}
else
{
System_printf ("Successfully configured Inbound Translation!\n");
}
if ((retVal = pcieObTransCfg (handle, PCIE_OB_LO_ADDR_S, PCIE_OB_HI_ADDR_S, PCIE_OB_REGION_S)) != pcie_RET_OK)
{
System_printf ("Failed to configure Outbound Address Translation!\n", (int)retVal);
exit(1);
}
else
{
System_printf ("Successfully configured Outbound Translation!\n");
}
}
System_printf ("Starting link training...\n");
/*Enable link training*/
if ((retVal = pcieLtssmCtrl(handle, TRUE)) != pcie_RET_OK)
{
System_printf ("Failed to Enable Link Training!\n", (int)retVal);
exit(1);
}
/* Wait for link to be up */
pcieWaitLinkUp(handle);
System_printf ("Link is up.\n");
if(PcieModeGbl == pcie_RC_MODE)
{
/**********************************************************************/
/* Push a single message to the EP then verify that it is echoed back */
/**********************************************************************/
/* Write from RC to EP */
if ((retVal = Pcie_getMemSpaceRange (handle, &pcieBase, NULL)) != pcie_RET_OK) {
System_printf ("getMemSpaceRange failed\n", (int)retVal);
exit(1);
}
for (i=0; i<PCIE_BUFSIZE_APP; i++)
{
*((volatile uint32_t *)pcieBase + i) = srcBuf[i];
}
/* Mark that the buffer is full, so EP can process it */
*((volatile uint32_t *)pcieBase + PCIE_BUFSIZE_APP) = PCIE_EXAMPLE_BUF_FULL;
/* Note on cache coherence: Write back is not necessary because pcieBase is in
peripheral address space instead of physical memory*/
/* Data sent to EP.
RC waits for the loopback to be completed and
receive data back from EP */
do {
unsigned int key;
/* Disable Interrupts */
key = _disable_interrupts();
/* Cleanup the prefetch buffer also. */
CSL_XMC_invalidatePrefetchBuffer();
CACHE_invL1d ((void *)dstBuf.buf, PCIE_EXAMPLE_DSTBUF_BYTES, CACHE_FENCE_WAIT);
CACHE_invL2 ((void *)dstBuf.buf, PCIE_EXAMPLE_DSTBUF_BYTES, CACHE_FENCE_WAIT);
/* Reenable Interrupts. */
_restore_interrupts(key);
} while(dstBuf.buf[PCIE_BUFSIZE_APP] != PCIE_EXAMPLE_BUF_FULL);
/* check all the data */
for (i=0; i<PCIE_BUFSIZE_APP; i++)
{
if(dstBuf.buf[i] != srcBuf[i])
{
System_printf ("Received data = %d\nTransmited data = %d\nIndex = %d.\n\nTest failed.\n",
dstBuf.buf[i], srcBuf[i], i);
exit(1);
}
}
System_printf ("Root Complex received data.\nTest passed.\n");
}
else
{
/**********************************************************************/
/* Wait for a single message from the RC then echo it back */
/**********************************************************************/
/* EP waits for the data received from RC */
do {
unsigned int key;
/* Disable Interrupts */
key = _disable_interrupts();
/* Cleanup the prefetch buffer also. */
CSL_XMC_invalidatePrefetchBuffer();
CACHE_invL1d ((void *)dstBuf.buf, PCIE_EXAMPLE_DSTBUF_BYTES, CACHE_FENCE_WAIT);
CACHE_invL2 ((void *)dstBuf.buf, PCIE_EXAMPLE_DSTBUF_BYTES, CACHE_FENCE_WAIT);
/* Reenable Interrupts. */
_restore_interrupts(key);
} while(dstBuf.buf[PCIE_BUFSIZE_APP] != PCIE_EXAMPLE_BUF_FULL);
System_printf ("End Point received data.\n");
/* Loopback to RC what was written in the DST buffer.
Write from EP to RC */
if ((retVal = Pcie_getMemSpaceRange (handle, &pcieBase, NULL)) != pcie_RET_OK) {
System_printf ("getMemSpaceRange failed\n", (int)retVal);
exit(1);
}
for (i=0; i<PCIE_BUFSIZE_APP; i++)
{
*((volatile uint32_t *)pcieBase + i) = dstBuf.buf[i];
}
/* Mark that the buffer is full, so RC can process it */
*((volatile uint32_t *)pcieBase + PCIE_BUFSIZE_APP) = PCIE_EXAMPLE_BUF_FULL;
/* Note on cache coherence: Write back is not necessary because pcieBase is in
peripheral address space instead of physical memory*/
System_printf ("End Point sent data to Root Complex, completing the loopback.\nEnd of Test.\n");
}
exit(0);
}
Thanks and regards,
Koichiro Tashiro