Part Number: AM625
Hello ,
1. Is it possible to use the MSRAM for the IPC shared memory ?
2. Which part of memory is advisable for the IPC Shared memory configuration ?
Currently there is no mention about the MSRAM in the AM62 TRM. On a different ticket, it was mentioned " There are other PSRAMs throughout the chip for use by other cores, but the 64K psram at base address 0x7000_0000 should be the equivalent to the 2MB msram on AM64 at base address 0x7000_0000. "
3. Does that mean MSRAM is 2MB in size ?