This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: Shared memory for IPC communication

Part Number: AM625

Hello ,

1. Is it possible to use the MSRAM for the IPC shared memory ?

2. Which part of memory is advisable for the IPC Shared memory configuration ?

Currently there is no mention about the MSRAM in the AM62 TRM. On a different ticket, it was mentioned " There are other PSRAMs throughout the chip for use by other cores, but the 64K psram at base address 0x7000_0000 should be the equivalent to the 2MB msram on AM64 at base address 0x7000_0000. 

3. Does that mean MSRAM is 2MB in size ?