Part Number: TDA4VM
The latest version of the TRM for j721E / TDA4VM (spruil1c / March 2022) is still lacking important parts of the McASP section, for instance:
- "Figure 12-485. MCASP Interface Signal" is empty
- "Figure 12-494. MCASP Integration" is empty
- "12.5.2.3.1 MCASP Integration in MAIN Domain" is missing vome values (marked by {X} and {Y} in the following paste: "There are MCASP {X} modules integrated in the device MAIN domain - . Figure 12-494 shows the integration of MCASP[0-{Y}]."
- in "Table 12-494. Global Initialization of Surrounding Modules" , several references to "Clocking" and "Interrupts" are lacking a precise section reference and hyperlink
are there any examples of McASP with the TDA4VM ?
- "Table 12-485. MCASP Clocks and Resets" references MCASPi_CLK and MCASPi_AUX_CLK modules, and I'd expect to find references to these elsewhere in the TRM, either in as MCASPi_CLK and MCASPi_AUX_CLK or as (e.g.") MCASP0_CLK and MCASP0_AUX_CLK form, but I cannot find any reference to either of these forms by searching the pdfs that make up the TRM.
When can we expect a production-ready version of this section?