This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: DDR init failure

Guru 10006 points

Part Number: AM3352
Other Parts Discussed in Thread: TPS65218D0, , TPS65217

Hi TI Champs

There's a request from Customer who met a boot failure on thier 1st custom board with AM3352 and TPS65218D0.

Their CPU board which referenced MYiR with TPS65217 works fine along with their separeated carrier board. 

However they attached TPS65218D0 which was recommended by TI earlier. and it still doen't work on their 1st costom board.

When they tried to attach JTAG trace, It unable to pass dram_init().

They could not figure out any problamatic point from their schematic.

Could you please check the interface btw AM3352 and DDR including PMIC TPS65218D0?

DTNS-MOD_REVA_DSN.pdf 

Also attached their cpatured power signal level.

  1. DCDC1(VDD_CORE/1.1V): 1.11V
  2. DCDC2(VDD_MPU/1.1V): 1.11V
  3. DCDC3(VDD_VDDQ_DDR/1.35V): 1.36V
  4. DCDC4(VDD_3P3/3.3V): 3.32V
  5. DCDC5(VDD_RTC/1V): 0.969V
  6. DCDC6(VDDS_RTC/1.8V): 1.79V
  7. LDO1(VDD_1P8/1.8V): 1.78V
  8. LS1(VDDS_DDR/1.35V): 1.33V

DTNS MPU_ PMIC TPS65218D0 voltage_level_220720.zip

Please check the schematic and voltage level captured from PMIC.

Thanks.

Regards, 

Jack