The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] 66AK2H12: U-Boot flash from CCS for K2HK / K2E family devices

Part Number: 66AK2H12

How to flash U-Boot from CCS for K2HK family devices ?

  • For flashing U-Boot from CCS, following pre-requisite needs to be done.

    For K2H EVM:

    1. Install CCS (https://www.ti.com/tool/download/CCSTUDIO/9.3.0.00012),
    2. Build U-Boot by following this FAQ - https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1115842/faq-66ak2h12-evmk2h-u-boot-build
    3. Create target configuration for K2H EVM by following this FAQ - https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1084886/faq-66ak2h12-target-configuration-in-ccs-for-k2h

    For K2E EVM:

    1. Install CCS (https://www.ti.com/tool/download/CCSTUDIO/9.3.0.00012),
    2. Build U-Boot by following this FAQ - [FAQ] 66AK2E05: How to build u-boot for K2E ? from the package "PROCESSOR-SDK-LINUX-K2E" - Processors forum - Processors - TI E2E support forums
    3. Create target configuration for K2E EVM by following this FAQ - [FAQ] 66AK2E05: How to create "Target configuration" and do "Test connection" on K2E EVM. - Processors forum - Processors - TI E2E support forums

    Now, Kindly follow the steps.

    1. In CCS, Open "Target Configuration" tab by  "View" -> "Target Configuration".
    2. Make sure the Device Boot mode is set at "DSP No-Boot", Kindly refer the K2H / K2E EVM Quick start guide.
      1. For K2H EVM
    3. 0714.EVMK2H_QSG_v2.pdf.
    4. For K2E EVM:
    5. 0763.EVMK2E_QuickSetupGuide.pdf
    6. Right click on "K2H" configuration for K2H EVM -or- K2E configuration for K2E EVM and select "Launch Selected Configuration".
    7. In the Debug window, Select the ARM core 0 "arm_A15_0" and select "Connect Target".
    8. Now, Select the core and go to "Tools > Load Memory",
      1. Select type as "TI Raw data" and Select "uboot.bin" file.
      2. In the next dialog, give start address as "0xc000000", type size as "32 bit" and swap "un checked".
    9. Go to "View -> Registers" and select the "Core register -> PC". Modify its value to "0xc000000".
    10. Now, select "Run -> Free Run".
    11. Connect through "Serial terminal" with following serial settings
      1. Baud rate : 115200
      2. Data bit    : 8
      3. Stop bit    : 1
      4. Parity       : None
      5. Flow control : None
    12. And, now U-boot runs on the RAM and flash it to the NOR memory by giving the following commands sequentially in the mentioned order (Also give commands either DHCP or static IP, do not give both commands)
      //Load default environment variables
      # env default -f -a
      
      //If device(EVM) IP address is set through dhcp 
      # setenv autoload no
      # dhcp
      
      //If device(EVM) IP address has to be set manually
      # setenv ipaddr 192.168.2.250
      # setenv gatewayip 192.168.2.1
      # setenv netmask 255.255.255.0
      
      //set tftp serer ip
      # setenv serverip 192.168.2.252
      
      //set name_uboot to file name "u-boot-spi.gph"
      # setenv name_uboot u-boot-spi.gph
      
      # saveenv							//make local variables into environment variables
      
      # ping ${serverip}
      
      # tftp ${loadaddr} ${serverip}:${name_uboot}
      
      # run burn_uboot_spi
    13. Here, TFTP server created using "Mobaxterm" software and U-boot moved from Linux PC to windows for ease.
    14. Refer this video for execution of steps,

    Also refer this URL for queries, https://github.com/ARM-software/u-boot/blob/master/board/ti/ks2_evm/README (Contents of the Link, if expired)

    k2hk_uboot_linux_flash.txt
    U-Boot port for Texas Instruments Keystone II EVM boards
    ========================================================
    
    Author: Murali Karicheri <m-karicheri2@ti.com>
    
    This README has information on the U-Boot port for K2HK, K2E, and K2L EVM boards.
    Documentation for this board can be found at
    http://www.advantech.com/Support/TI-EVM/EVMK2HX_sd.aspx
    https://www.einfochips.com/index.php/partnerships/texas-instruments/k2e-evm.html
    https://www.einfochips.com/index.php/partnerships/texas-instruments/k2l-evm.html
    
    The K2HK board is based on Texas Instruments Keystone2 family of SoCs: K2H, K2K.
    More details on these SoCs are available at company websites
     K2K: http://www.ti.com/product/tci6638k2k
     K2H: http://www.ti.com/product/tci6638k2h
    
    The K2E SoC details are available at
     http://www.ti.com/lit/ds/symlink/66ak2e05.pdf
    
    The K2L SoC details are available at
     http://www.ti.com/lit/ds/symlink/tci6630k2l.pdf
    
    The K2G SoC details are available at
     http://www.ti.com/lit/ds/symlink/66ak2g02.pdf
    
    Board configuration:
    ====================
    
    Some of the peripherals that are configured by U-Boot
    +------+-------+-------+-----------+-----------+-------+-------+----+
    |      |DDR3   |NAND   |MSM SRAM   |ETH ports  |UART   |I2C    |SPI |
    +------+-------+-------+-----------+-----------+-------+-------+----+
    |K2HK  |2      |512MB  |6MB	   |4(2)       |2      |3      |3   |
    |K2E   |4      |512MB  |2MB	   |8(2)       |2      |3      |3   |
    |K2L   |2      |512MB  |2MB	   |4(2)       |4      |3      |3   |
    |K2G   |2      |256MB  |1MB	   |1          |1      |1      |1   |
    +------+-------+-------+-----------+-----------+-------+-------+----+
    
    There are only 2 eth port installed on the boards.
    
    There are separate PLLs to drive clocks to Tetris ARM and Peripherals.
    To bring up SMP Linux on this board, there is a boot monitor
    code that will be installed in MSMC SRAM. There is command available
    to install this image from U-Boot.
    
    The port related files can be found at following folders
     keystone2 SoC related files: arch/arm/cpu/armv7/keystone/
     EVMs board files: board/ti/k2s_evm/
    
    Board configuration files:
    include/configs/k2hk_evm.h
    include/configs/k2e_evm.h
    include/configs/k2l_evm.h
    include/configs/k2g_evm.h
    
    As U-Boot is migrating to Kconfig there is also board defconfig files
    configs/k2e_evm_defconfig
    configs/k2hk_evm_defconfig
    configs/k2l_evm_defconfig
    configs/k2g_evm_defconfig
    
    Supported boot modes:
     - SPI NOR boot
     - AEMIF NAND boot (K2E, K2L and K2HK)
     - UART boot
     - MMC boot (Only on K2G)
    
    Supported image formats:
     - u-boot.bin: for loading and running u-boot.bin through
    		Texas Instruments code composure studio (CCS) and for UART boot.
     - u-boot-spi.gph: gpimage for programming SPI NOR flash for SPI NOR boot
     - MLO: gpimage for programming NAND flash for NAND boot, MMC boot.
    
    Build instructions:
    ===================
    Examples for k2hk, for k2e, k2l and k2g just replace k2hk prefix accordingly.
    Don't forget to add ARCH=arm and CROSS_COMPILE.
    
    To build u-boot.bin, u-boot-spi.gph, MLO:
      >make k2hk_evm_defconfig
      >make
    
    Load and Run U-Boot on keystone EVMs using CCS
    =========================================
    
    Need Code Composer Studio (CCS) installed on a PC to load and run u-boot.bin
    on EVM. See instructions at below link for installing CCS on a Windows PC.
    http://processors.wiki.ti.com/index.php/MCSDK_UG_Chapter_Getting_Started#
    Installing_Code_Composer_Studio
    Use u-boot.bin from the build folder for loading and running U-Boot binary
    on EVM. Follow instructions at
    K2HK http://processors.wiki.ti.com/index.php/EVMK2H_Hardware_Setup
    K2E  http://processors.wiki.ti.com/index.php/EVMK2E_Hardware_Setup
    K2L  http://processors.wiki.ti.com/index.php/TCIEVMK2L_Hardware_Setup
    K2G  http://processors.wiki.ti.com/index.php/66AK2G02_GP_EVM_Hardware_Setup
    
    to configure SW1 dip switch to use "No Boot/JTAG DSP Little Endian Boot Mode"
    and Power ON the EVM.  Follow instructions to connect serial port of EVM to
    PC and start TeraTerm or Hyper Terminal.
    
    Start CCS on a Windows machine and Launch Target
    configuration as instructed at http://processors.wiki.ti.com/index.php/
    MCSDK_UG_Chapter_Exploring#Loading_and_Running_U-Boot_on_EVM_through_CCS.
    The instructions provided in the above link uses a script for
    loading the U-Boot binary on the target EVM. Instead do the following:-
    
    1. Right click to "Texas Instruments XDS2xx USB Emulator_0/CortexA15_1 core (D
       is connected: Unknown)" at the debug window (This is created once Target
       configuration is launched) and select "Connect Target".
    2. Once target connect is successful, choose Tools->Load Memory option from the
       top level menu. At the Load Memory window, choose the file u-boot.bin
       through "Browse" button and click "next >" button. In the next window, enter
       Start address as 0xc000000, choose Type-size "32 bits" and click "Finish"
       button.
    3. Click View -> Registers from the top level menu to view registers window.
    4. From Registers, window expand "Core Registers" to view PC. Edit PC value
       to be 0xc000000. From the "Run" top level menu, select "Free Run"
    5. The U-Boot prompt is shown at the Tera Term/ Hyper terminal console as
       below and type any key to stop autoboot as instructed :=
    
    U-Boot 2014.04-rc1-00201-gc215b5a (Mar 21 2014 - 12:47:59)
    
    I2C:   ready
    Detected SO-DIMM [SQR-SD3T-2G1333SED]
    DRAM:  1.1 GiB
    NAND:  512 MiB
    Net:   K2HK_EMAC
    Warning: K2HK_EMAC using MAC address from net device
    , K2HK_EMAC1, K2HK_EMAC2, K2HK_EMAC3
    Hit any key to stop autoboot:  0
    
    SPI NOR Flash programming instructions
    ======================================
    U-Boot image can be flashed to first 512KB of the NOR flash using following
    instructions:
    
    1. Start CCS and run U-Boot as described above.
    2. Suspend Target. Select Run -> Suspend from top level menu
       CortexA15_1 (Free Running)"
    3. Load u-boot-spi.gph binary from build folder on to DDR address 0x87000000
       through CCS as described in step 2 of "Load and Run U-Boot on K2HK/K2E/K2L
       EVM using CCS", but using address 0x87000000.
    4. Free Run the target as described earlier (step 4) to get U-Boot prompt
    5. At the U-Boot console type following to setup U-Boot environment variables.
       setenv addr_uboot 0x87000000
       setenv filesize <size in hex of u-boot-spi.gph rounded to hex 0x10000>
       run burn_uboot_spi
       Once U-Boot prompt is available, Power OFF the EVM. Set the SW1 dip switch
       to "SPI Little Endian Boot mode" as per instruction at
       http://processors.wiki.ti.com/index.php/*_Hardware_Setup.
    6. Power ON the EVM. The EVM now boots with U-Boot image on the NOR flash.
    
    AEMIF NAND Flash programming instructions
    ======================================
    U-Boot image can be flashed to first 1024KB of the NAND flash using following
    instructions:
    
    1. Start CCS and run U-Boot as described above.
    2. Suspend Target. Select Run -> Suspend from top level menu
       CortexA15_1 (Free Running)"
    3. Load MLO binary from build folder on to DDR address 0x87000000
       through CCS as described in step 2 of "Load and Run U-Boot on K2HK EVM
       using CCS", but using address 0x87000000.
    4. Free Run the target as described earlier (step 4) to get U-Boot prompt
    5. At the U-Boot console type following to setup U-Boot environment variables.
       setenv filesize <size in hex of MLO rounded to hex 0x10000>
       run burn_uboot_nand
       Once U-Boot prompt is available, Power OFF the EVM. Set the SW1 dip switch
       to "ARM NAND Boot mode" as per instruction at
       http://processors.wiki.ti.com/index.php/*_Hardware_Setup.
    6. Power ON the EVM. The EVM now boots with U-Boot image on the NAND flash.
    
    Load and Run U-Boot on keystone EVMs using UART download
    ========================================================
    
    Open BMC and regular UART terminals.
    
    1. On the regular UART port start xmodem transfer of the u-boot.bin
    2. Using BMC terminal set the ARM-UART bootmode and reboot the EVM
       BMC> bootmode #4
       MBC> reboot
    3. When xmodem is complete you should see the U-Boot starts on the UART port
    
    Load and Run U-Boot on K2G EVMs using MMC
    ========================================================
    
    Open BMC and regular UART terminals.
    
    1. Set the SW3 dip switch to "ARM MMC Boot mode" as per instruction at
       http://processors.wiki.ti.com/index.php/66AK2G02_GP_EVM_Hardware_Setup
    2. Create SD card partitions as per steps given in Hardware Setup Guide.
    3. Copy MLO to Boot Partition.
    4. Insert SD card and Power on the EVM.
       The EVM now boots with U-Boot image from SD card.

    Thanks & Regards,

    Rajarajan U