Hi:
Just to put this up top, this issue is preventing me from building SDK 08.
Having to rebuild my tisdk directory. Have not had to do that for some time, and having many issues with links to git not working, and fetching not working.
Early this year I never had these kinds of issues, but I was hoping to use the "Using source package snapshot" instructions to get around my build problems.
I found this thread which I must say I agree with. This section really needs fixing. The instructions are wrong for both 07 and 08 SDK version docs.
The step-by-step (no steps in red), kind of imply that the file I need to download is of the form:
<target-board>-linux-sdk-arago-src-##.##.##.##.tar.xz
When I go to the downloads directory for 07 I see this file which seems right:
am437x-evm-linux-sdk-arago-src-07.03.00.005.tar.xz
When I go to the downloads directory for 08 the file does not exist.
The downloads dir I have is this:
https://www.ti.com/tool/download/PROCESSOR-SDK-LINUX-AM437X/08.02.00.24
I was playing around with getting 08 to build to see if I wanted to move from 07 to 08,
but I can't get 08 to build due to failures in mobile-broadband-provider,
which is why I was trying the source snapshot. See this thread:
e2e.ti.com/.../processor-sdk-am437x-mobile-broadband-provider-fetcher-failure-in-clean-08-build
This issue is blocking me from building 08, and currently there are other issues building 07 (see END of the thread below), so I am totally blocked at the moment.
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1127235/processor-sdk-am437x-links-to-am437-sdk-version-07-documentation-and-sdk-links-are-all-broken