Part Number: AM3358
Hi I need to communicate two slaves using gpmc if i use read and write signal for both is any Collison happen in data or I can use other gpios for fpga to read and write pin?
thank you
suguresh M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM3358
Hi I need to communicate two slaves using gpmc if i use read and write signal for both is any Collison happen in data or I can use other gpios for fpga to read and write pin?
thank you
suguresh M
Hello suguresh
Thank you for the query
The GPMC interface allows connecting to multiple devices through chip selects.
it is recommended to perform simulation before implementation ad provision for series/parallel terminations that may be required.
Regards,
Sreenivasa
Hello Suguresh
Although not related, the below thread could be used as a reference to understand the effect of routing and terminations.
Please check if you are following the guidelines mentioned in the processor design review checklist along with the recommendations by the other devices.
Regards,
Sreenivasa
ok if i need more address i can assign and use in non mux mode? because in ref manual only 27bit address is there.
thank you
suguresh M
Hello Suguresh,
Thank you for the message.
I am not able to understand your comment fully. Could you please point me to the TRM section you are referring.
Regards,
Sreenivasa
I'm using non mux type and if i use from gpmc_0 to gpmc_26.is it works ? and if i want still more address i can take or 27 bit address is fixed?
thank you
suguresh M
Hello Suguresh,
Thank you for the note. Please check the address bits connection.
If the problem persists please share the interface diagram.
Regards,
Sreenivasa