This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM-Q1: TDA4VL Boot mode configuation

Part Number: TDA4VM-Q1

hi team,

    if i need the configuration of primary EMMC boot and backup MMC/SD card boot. do i need to configure the port number? do i need to configure the bootmode[6] to 0, and bootmode[7] to 1? 

  • Hi,

    Section 4 Initialization, of the TRM contains subsections on supported boot modes.  Please refer to this documentation.

    From above yes, "bootmode[6] to 0, and bootmode[7] to 1" , appears correct, recommend testing on EVM.

    Regards,

    kb