Hi,
i am using Blackhawk XDS560v2-USB System Trace Emulator with CCSv10.
OS : Linux 18.04.1-Ubuntu 64bit
Processor : AM3359
but i am getting following error as after test connection. can you suggest how can i solve this error??
[Start: Blackhawk XDS560v2-USB System Trace Emulator_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
/home/jayesh/.ti/ccs1000/0/0/BrdDat/testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'libbh560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: open failed: code 19
Download failed for file /home/jayesh/ti/ccs1000/ccs/ccs_base/common/uscif/./././././xds560v2.out
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.
[End: Blackhawk XDS560v2-USB System Trace Emulator_0]
thanks & regard,
Gajanan Shete