This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: XDS110 Debug

Part Number: TDA4VM


1   In CCS10.4.0.00006_WIN64, TDA4 OFFICIAL BOARD, XDS110 USB DEBUG environment, how do I download and burn: *.  Out file.   Please help me confirm whether my method is correct (see the attached document).   Error (Error: -261@0xffffFefb)/(error: -261@0) for unknown reasons.   I have set the SD card mode dial the code switch, and I put the following three files Sysfw.  Bin/tiboot3.  Bin/app has been copied to the SD card.创建工程过程.docx2    And I will have a phenomenon when burning the program, connect TDA4 board, my desktop computer screen will be disturbed, has been flashing, and my keyboard can not input typing, turn off the development board power can be。

  • Hi Chen,

    Can you please elaborate on the use case here? The procedure shared in the document is not correct. If you want to load the .out from debugger, you should do that in no-boot mode and you do not need to run SBL and TIFS from SD Card. If you want to load from SD boot then you should load the binary from SD Card itself.

    Also, if you are connecting to target via CCS after running SBL via SD Card, you should not run the launch.js or any GEL script.

    Regards,
    Parth