Hi,
We're working on the block diagram for a new board that includes a C6455 and at present SRIO boot is fundamental to our design.
We want to go to fix the design pretty soon and I was asked if I could guarantee that there aren't any problems with SRIO boot. I said "I'm sure it will be fine"! I don't yet know much about SRIO and was hoping someone could confirm that it will be fine.
We only intend to connect one of the channels (port0 I guess) and want to use 1.25Gb/s.
Unfortunately I'm not sure I fully understand the difference between 4 1x ports and 1 4x port. I'm hoping that 4 1x ports (boot configuration 0) means that port 0 will work on it's own and it doesn't matter that the other 3 are not connected to the host.
Any comments about SRIO would be boot greatfully received!
Thanks,
Matt