This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Our custom board required two LVDS Displays. The AM625 datasheet mentions LVDS -1 (8x Lane).
If possible use 2 LVDS displays using 4 lanes for display 1 and another four-lane for display 2 ???
Regards
Pandian
Hello Pandian,
Yes, it's possible to connect two displays and use the LVDS in single link mode. However, due to HW limitations, both the displays will be mirrored.
Regards,
Krunal
Hi Krunal,
Thanks for your reply.
If two displays we used at the same time can I play two different videos are not ???
Regards
Pandian
Hello,
Thank for your reply krunal
If I used HDMI and LVDS Display at the same time both display will support 2K resolutions are not ???
Regards
pandian
Hello,
Yes, both DPI and LVDS have independent PLL so it's possible to run both at 1080p60 resolutions. However, please keep in mind that we only have 16bit DDR on AM62x. The displays will run at 60FPS because of VSYNC but GPU/A53 FPS will vary based on the load.
Regards,
Krunal