Other Parts Discussed in Thread: 66AK2H06
Dear Sir,
is 66K2H06 DSP having feature to ethernet? is any sample code, I can refer?
Thanks,
Yao-Ting
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: 66AK2H06
Dear Sir,
is 66K2H06 DSP having feature to ethernet? is any sample code, I can refer?
Thanks,
Yao-Ting
Hi Yao,
is 66K2H06 DSP having feature to ethernet? is any sample code, I can refer?
Yes, Ethernet sample projects for DSP core are available in PDK.
https://www.ti.com/tool/download/PROCESSOR-SDK-RTOS-K2HK (Download the latest stable version)
Kindly refer to the following FAQs.
Thanks
Rajarajan U
Hi Rajarajan,
I am in the windows system.
i follow the instruction to generate projects. pdksetupenv.bat is ok
However, when i execute pdkProjectCreate.bat. it says the system cannot find patch specified.
what should I do to make it generates projects?

Thank you.
Yao-Ting
Hi Yao-Ting,
In the command prompt, give the commands as per the FAQ. In the path "C:\ti\pdk_k2hk_4_0_16\packages" give "pdksetupenv.bat" and then "pdkProjectCreate.bat K2H all little all all dsp "C:\ti\pdk_k2hk_4_0_16\packages"".
The PDK projects will be created inside the C:\ti\pdk_k2hk_4_0_16\packages folder.
And, Do not use the command "pdkProjectCreate.bat" without any arguments.
Thanks
Rajarajan U
(If the issue is resolved, kindly press the "This resolved my issue" green button.
Hi Rajaraja.
here is what i got.

in the end, no folder is created.

Thank you for help.
Yao-Ting
Hi Yao,
Have you installed the Code Composer studio? Once CCS was installed, open CCS and it will automatically detects the SDK installation and also updates the "Tools" from SDK.
After then, Try this commands. Project creation uses CCS to generate projects.
Thanks
Rajarajan
Hi Rajarajan,
i am using 66Ak2h06 and try to generate the projects.
However, i cannot find it from pop down manual. which board, i should select?
thank you.

Yao-Ting
Yao-TIng,
Pre-requisite
Follow the steps given here. Kindly install the same version mentioned in the link. I.e., CCS 9.3
and then post the screenshot of each step.
Regards
Shankari G
Hi Shankari,
here are my steps.
install PROCESSOR-SDK-RTOS-K2HK 06_03_00_106

install 9.3 CCS

use the default folder or default setting and products select 66Ak2x




open CCS 9.3 and let it updates.
set the environments

set pdkProjectsCreate.bat

there is no error, but it looks it doesn't generate projects in my computer.
Thank you for the help.
Yao-Ting
Hi Yao-Ting,
Please try the following,
Install the K2HK RTOS SDK with following options enabled,
66AK2X Multicore DSP + ARM
C6000 Power optimized DSP
C64x Multicore DSP
Enable Blackhawk debug probe
Before giving the commands on Command prompt, Please open the CCS and go to Window -> Preferences -> Code Composer Studio -> Products and it will show like this,
Thanks
Rajarajan U
Hi Rajarajan,
I install CCS 9.3
66AK2X Multicore DSP + ARM
C6000 Power optimized DSP
Enable Blackhawk debug probe


here is Window -> Preferences -> Code Composer Studio ->products

and the result is still the same.

is it possible my PC already install CCS 11 before, that makes CCS 9 setting up environment wrong?
Thank you,
Yao-Ting
Yao-Ting,
If that is the case, uninstall CCS11 and reinstall CCS 9.3.
Regards
Shankari G
Thank you. After I uninstall CCS11 and reinstall PROCESSOR-SDK-RTOS-K2HK 06_03_00_106 and reinstall CCS 9.3, it works.
Congrats, Yao-Ting,
Glad to hear. Marking the thread status as closed.
Regards
Shankari G