Part Number: AM6412
Hi TI,
How to generate USB compliance test from CPU In Linux kernel 5.10 on AM64xx.
I followed the instructions below.
TDA4VM: USB 2.0 host test mode
Set dr_mode to host.
# cat /proc/device-tree/bus\@f4000/cdns-usb\@f900000/usb\@f400000/dr_mode
host
# cat /proc/device-tree/bus\@f4000/cdns-usb\@f900000/usb\@f400000/compatible
cdns,usb3
Unbind the usb 2.0 hub befind CPU.
# echo '1-1' > /sys/bus/usb/drivers/usb/unbind
# lsusb -t
/: Bus 02.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 5000M
/: Bus 01.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 480M
And, type the command to generate the test pattern.
# echo compliance > /sys/kernel/debug/usb/xhci/xhci-hcd.1.auto/ports/port01/portsc
# cat /sys/kernel/debug/usb/xhci/xhci-hcd.1.auto/ports/port01/portsc
PORTSC = 0xc000e63
Powered Connected Enabled Link:U3 PortSpeed:3 Change: Wake: WDE WOE
However, The CPU doesn't seem to generate any signals.
What are we missing here?
Or, is there any other way to generate test patterns?
Thanks,
Sean