Part Number: TMS320C6678
CCS version: 9.3
SDK version: 06_03_00_106
Board: TMS320C6678LE
I am running the "NIMU_emacClientExample_EVMC6678C66BiosExampleProject" and getting to the point where the DHCP client is waiting to be discovered, but the server is not providing a DHCP offer. I'm using Wireshark to observe what is being sent out. Does anyone have any suggestions on what I could do? Do I need to make changes to the client.c file?
I tried also tried changing the program from using a DHCP connection to a static IP connection, and the IP shows up on the console, but I can't get the demo website to open. I could use any help that I can get.
I tried this out on my work laptop and personal laptop and got the same results. I am using No Boot mode, and I even tried flipping the last switch off when I changed modes.