Other Parts Discussed in Thread: CCSTUDIO
Hi,
Would you please provide a "Quick set up Guide or development guide or start up guide for C6678 and C6678-EVM " to enable a quick product development ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Would you please provide a "Quick set up Guide or development guide or start up guide for C6678 and C6678-EVM " to enable a quick product development ?
Master-FAQ List – C6678 and C6678-EVM
Introduction:
This Master-FAQ document will help to explore the functions and features of C6678 Processor device using the C6678-Evaluation Module(EVM) with SDK. Going through these FAQ-list will help the customer to get good hands-on experience on the C6678-EVM and help for a smoother and quicker navigation to their customized product development.

Content-List
For hassle-free experience, user is requested to follow the steps sequentially.
1.The Latest SDK –
There are many versions of SDK released for C6678 processor. When this document is written, this is the latest.
|
SDK NAME |
Download link |
|
PROCESSOR-SDK-RTOS-C667x 06_03_00_106 |
For older versions of SDK, visit https://www.ti.com/tool/PROCESSOR-SDK-C667X
Click --> "Download" --> Previous versions https://www.ti.com/tool/download/PROCESSOR-SDK-RTOS-C667X#previous-versions
Please ensure, the revision number of C6678-EVM matches with the SDK version ( here 6.3 is used ) .
2.The (IDE) Integrated development environment –
As the PROCESSOR-SDK-RTOS-C667x 06_03_00_106 is tested to run successfully in CCS version 9.3.0.00012 without any errors, the users are recommended to stick to this CCS version.
However, the user, may use, the higher versions of CCS, as their own choice. TI could not guarantee solution, if errors faced while using in-compatible versions of CCS with SDK.
|
IDE NAME |
Download link |
|
CCSTUDIO_9.3.0.00012
|
https://www.ti.com/tool/download/CCSTUDIO/9.3.0.00012
|
3. How to run the out-of-box-demo of C6678 EVM
In your C6678 EVM - board ----> You should put the DIP Switch settings in "No boot mode" to connect to the CCS.
That is ------> DIP SW 3,4,5 and 6 like given below.

4.How to make use of the SDK with IDE and EVM
In your C6678 EVM - board ----> You should put the DIP Switch settings in "No boot mode" to connect to the CCS.
That is ------> DIP SW 3,4,5 and 6 like given below.

4.a) How to set the development environment and establish the connection between the EVM and the development-PC.
|
Purpose |
FAQ-link |
|
How to create "Target configuration" and do "Test connection" on C6678 EVM |
|
|
How to load and run the DSP gel file on C6678 EVM |
4.b) How to generate the CCS-based PDK examples.
4.c) How to rebuild the PDK and SDK examples.
4.d) How to build and run the platform test on C6678 EVM ?
The same steps are captured in the video below:
4.e) How to build the IBL –
Please note: The building steps are given for C665x. Please provide “C6678” as device parameter in place of C665x , while building
|
Build environment |
Steps in FAQ links |
|
Using Windows 10 |
|
|
Using Linux |
4.f) How to flash the IBL (Intermediate Boot loader) into EEPROM and how to flash the application binary into NOR? How to boot the IBL + Application.
4.g) How to build and run the IPC example on C6678 EVM.
The same steps are captured in the video below:
5. How to run TSIP example on C6678 EVM?
6. How to run NIMU-EMAC client example on C6678 EVM?
Other Important Links and resources
C6678-EVM
Where to buy : https://www.ti.com/tool/TMDSEVM6678
Schematics and other hardware docs: https://www2.advantech.com/Support/TI-EVM/6678le_sd.aspx
C6678 Processor:
About the functions and features of C6657 processor - Product folder : https://www.ti.com/product/TMS320C6678
Where to order :https://www.ti.com/product/TMS320C6678
Data sheet : https://www.ti.com/lit/ds/symlink/tms320c6678.pdf
Technical documentations - https://www.ti.com/product/TMS320C6678#tech-docs
Design and Development :https://www.ti.com/product/TMS320C6678#design-development
Software - https://www.ti.com/product/TMS320C6678#software-development
hardware - https://www.ti.com/product/TMS320C6678#hardware-development
If you have questions about quality, packaging or ordering TI products, see TI support.
To post a technical query on E2E Forum:(+) TI E2E support forums
Regards
Shankari G