This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: AM64x Ethercat & PTP PRU signals

Part Number: AM6442

Der Sitara team,

Additionnal question related to the previous one  about PTP support on AM64x :

Question 4/ We understand that Ethercat stack is only supported ond TI-RTOS and not on linux ? Do you confirm ?

Ethercat is able to generate sync signals in a similar way as PTP with the PPS signals. it seems like that PRU ethercat is able to generate output signal too but ...

Question 5/ is it possible to generate both 1Hz and 4800Hz with Ethercat PRU?

Thank you !

Best regards,

Guillaume