Hi,
I can't generate example project.
What is the problem ?
Regards,
Yakov Filiarsky.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I can't generate example project.
What is the problem ?
Regards,
Yakov Filiarsky.
Yakov,
In your fourth step, the path is missing.
In your snapshot, Your PDK_SHORT_NAME seems to be incorrect.
Second point: Have you installed the CCS 9.3? Because, this script will work only with CCS 9.3
Regards
Shankari G
Hi Shankari ,
You are correct, I use CCS 11.
I just changed the CCS location variable in pdkProjectCreate.bat to be CCS11. Now it works :-)
Yakov,
As some sample/example app of processor SDK 6.3 might not be expected to work with a normal behaviour with CCS 11.
CCS 9.3 is "THE" compatible and recommended version for Processor SDK 6.3
So, it is better to stick to CCS 9.3 ( Though I understand it might be deceiving, not to use the latest version of CCS )
Even on the first hand, the gel file needs modification here and there on the delay-codes, if you use CCS 11.
Then it is upto you!.
Happy journey with TI-processor.
Regards
Shankari G