Hello,
I have been looking for hours on an answer but could not find one. Here is my question:
I have a custom DM365 board that has been tested and is working fine with Linux, etc.
Until now, I have been using a micro-B USB cable connected to a desktop PC to power and communicate with the board and I had no problems. I tried using a micro-A USB and same result, the circuit is on and Linux is booting.
Now here is where I have a problem: when using a USB battery (for example the New Trent), the circuit is ON (DM365 is powered as usual) but Linux is not booting. I don't see anything on the serial line: no UBL, bootloader or Linux. Simply blank. Usually there should be a LED switching on (I programmed that into my code) but here nothing...
Where is the problem? If the program is not booting, is there a miscommunication on the USB line? The only difference I see between the USB coming from the desktop and USB coming from the battery is on the USB_P / USB_N or USB_ID lines. The battery probably does not have these 3 lines.
I have attached the schematics of my circuit (DM365 <-> USB).
Please let me know what you think.
Thanks!
Mike