Hi experts
SoC: TDA4VE
SDK: 8.4
EVM: J721S2 EVM
Does the ECO encode module support the use of high 32-bit memory addresses ? Such as 0x880 000 000
Best regards
Li quan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi experts
SoC: TDA4VE
SDK: 8.4
EVM: J721S2 EVM
Does the ECO encode module support the use of high 32-bit memory addresses ? Such as 0x880 000 000
Best regards
Li quan
Hi li,
The driver supports 48-bit addressing. You can use higher 32 bit memory addresses but it is disabled by default.
Please refer the below thread on how to enable 48bit addressing for higher 32 bit allocations.
e2e.ti.com/.../tda4vm-whether-encode-driver-can-use-high-32-bit-memory
Regards
Nikshith