Part Number: PROCESSOR-SDK-AM62X
Hi,
I am trying to run the gpio_leds.sh on EVM but it keeps failing due to not having any file in the /sys/class/leds/.
Both dts and defconfig are the default of the sdk (ti-processor-sdk-linux-am62xx-evm-08.04.01.03).
Host linux version: Ubuntu 20.04.5 LTS
Evm: am62xx-evm
CONFIG_NEW_LEDS=y CONFIG_LEDS_CLASS=y CONFIG_LEDS_GPIO=y CONFIG_LEDS_PWM=y CONFIG_LEDS_SYSCON=y CONFIG_LEDS_TRIGGER_TIMER=y CONFIG_LEDS_TRIGGER_DISK=y CONFIG_LEDS_TRIGGER_HEARTBEAT=y CONFIG_LEDS_TRIGGER_CPU=y CONFIG_LEDS_TRIGGER_DEFAULT_ON=y CONFIG_LEDS_TRIGGER_PANIC=y
// SPDX-License-Identifier: GPL-2.0
/*
* AM62x LP SK
*
* Copyright (C) 2021-2022 Texas Instruments Incorporated - https://www.ti.com/
*/
/dts-v1/;
#include <dt-bindings/leds/common.h>
#include <dt-bindings/gpio/gpio.h>
#include <dt-bindings/net/ti-dp83867.h>
#include "k3-am625.dtsi"
#include "k3-am62x-sk-common.dtsi"
/ {
compatible = "ti,am625-sk", "ti,am625";
model = "Texas Instruments AM62x LP SK";
wlan_lten: regulator-5 {
compatible = "regulator-fixed";
regulator-name = "wlan_lten";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
vin-supply = <&vcc_3v3_sys>;
gpios = <&exp2 9 GPIO_ACTIVE_LOW>;
};
wlan_en: regulator-6 {
/* OUTPUT of SN74AVC2T244DQMR */
compatible = "regulator-fixed";
regulator-name = "wlan_en";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
enable-active-high;
vin-supply = <&wlan_lten>;
gpios = <&main_gpio0 71 GPIO_ACTIVE_HIGH>;
pinctrl-names = "default";
pinctrl-0 = <&wlan_en_pins_default>;
};
};
&main_pmx0 {
wlan_en_pins_default: wlan-en-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x124, PIN_OUTPUT, 7) /* (A23) MMC2_SDCD.GPIO0_71 */
>;
};
main_mmc2_pins_default: main-mmc2-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x120, PIN_INPUT, 0) /* (C24) MMC2_CMD */
AM62X_IOPAD(0x118, PIN_INPUT, 0) /* (D25) MMC2_CLK */
AM62X_IOPAD(0x114, PIN_INPUT, 0) /* (B24) MMC2_DAT0 */
AM62X_IOPAD(0x110, PIN_INPUT, 0) /* (C25) MMC2_DAT1 */
AM62X_IOPAD(0x10c, PIN_INPUT, 0) /* (E23) MMC2_DAT2 */
AM62X_IOPAD(0x108, PIN_INPUT, 0) /* (D24) MMC2_DAT3 */
AM62X_IOPAD(0x11c, PIN_INPUT, 0) /* (#N/A) MMC2_CLKB */
>;
};
main_wlirq_pins_default: main-wlirq-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x128, PIN_INPUT, 7) /* (B23) MMC2_SDWP.GPIO0_72 */
>;
};
};
&main_i2c1 {
exp1: gpio@22 {
compatible = "ti,tca6424";
reg = <0x22>;
gpio-controller;
#gpio-cells = <2>;
gpio-line-names = "GPIO_CPSW2_RST", "GPIO_CPSW1_RST",
"PRU_DETECT", "MMC1_SD_EN",
"VPP_LDO_EN", "EXP_PS_3V3_En",
"EXP_PS_5V0_En", "EXP_HAT_DETECT",
"GPIO_AUD_RSTn", "GPIO_eMMC_RSTn",
"UART1_FET_BUF_EN", "BT_UART_WAKE_SOC",
"GPIO_HDMI_RSTn", "CSI_GPIO0",
"CSI_GPIO1", "GPIO_OLDI_INT",
"HDMI_INTn", "TEST_GPIO2",
"MCASP1_FET_EN", "MCASP1_BUF_BT_EN",
"MCASP1_FET_SEL", "UART1_FET_SEL",
"", "IO_EXP_TEST_LED";
interrupt-parent = <&main_gpio1>;
interrupts = <23 IRQ_TYPE_EDGE_FALLING>;
interrupt-controller;
#interrupt-cells = <2>;
pinctrl-names = "default";
pinctrl-0 = <&main_gpio1_ioexp_intr_pins_default>;
};
exp2: gpio@23 {
compatible = "ti,tca6424";
reg = <0x23>;
gpio-controller;
#gpio-cells = <2>;
gpio-line-names = "", "",
"", "",
"", "",
"", "",
"WL_LT_EN", "CSI_RSTz",
"", "",
"", "",
"", "",
"SPI0_FET_SEL", "SPI0_FET_OE",
"GPIO_OLDI_RSTn", "PRU_3V3_EN",
"", "",
"CSI_VLDO_SEL", "SOC_WLAN_SDIO_RST";
};
};
/*
* All SoC variants with the AMC package have no PRU.
* Attempting to access the PRU on these devices will
* result in a crash at kernel bootup.
*
* For now, we do not have any code that can figure out
* the absence of the PRU by reading any SoC registers,
* so for now disable the PRU here in the board DTS file.
*/
&pruss {
status = "disabled";
};
&sdhci2 {
status = "disabled";
};
&cpsw_port2 {
status = "disabled";
};
&cpsw3g_mdio {
cpsw3g_phy1: ethernet-phy@1 {
status = "disabled";
};
};
&ospi0 {
flash@0 {
compatible = "spi-nand";
reg = <0x0>;
spi-tx-bus-width = <8>;
spi-rx-bus-width = <8>;
spi-max-frequency = <25000000>;
cdns,tshsl-ns = <60>;
cdns,tsd2d-ns = <60>;
cdns,tchsh-ns = <60>;
cdns,tslch-ns = <60>;
cdns,read-delay = <2>;
cdns,phy-mode;
partitions {
compatible = "fixed-partitions";
#address-cells = <1>;
#size-cells = <1>;
partition@0 {
label = "ospi.tiboot3";
reg = <0x0 0x80000>;
};
partition@80000 {
label = "ospi.tispl";
reg = <0x80000 0x200000>;
};
partition@280000 {
label = "ospi.u-boot";
reg = <0x280000 0x400000>;
};
partition@680000 {
label = "ospi.env";
reg = <0x680000 0x40000>;
};
partition@6c0000 {
label = "ospi.env.backup";
reg = <0x6c0000 0x40000>;
};
partition@800000 {
label = "ospi.rootfs";
reg = <0x800000 0x77c0000>;
};
partition@3fc0000 {
label = "ospi.phypattern";
reg = <0x7fc0000 0x40000>;
};
};
};
};