Part Number: SK-AM62
I have received two AM62x Low Power SKEVM PROC124E1 boards from our TI Rep. (SL#09221240018)
I am not able to get Linux booted on them.
I have followed the guide: https://dev.ti.com/tirex/explore/node?node=A__AHfuoVse3tNf0ejVDqHu9A__am62x-devtools__FUz-xrs__LATEST&search=am62x
The image put on the SD-card is: https://dr-download.ti.com/software-development/software-development-kit-sdk/MD-PvdSyIiioq/08.04.01.09/tisdk-default-image-am62xx-evm.wic.xz
I have set the dip switches according to the guide. There was a mention of differences between E1 and E2 and I am not sure what version I have as my dip switches are named sw3 and sw4 (sw1 and sw2) in the document.
SW4: 01000000
SW2: 11000010
This is what I do get on the ttyUSB0 with thee above dip switches. Nothing more after.
U-Boot SPL 2021.01-g1c0d06c606 (Nov 07 2022 - 06:22:13 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.4.7--v08.04.07 (Jolly Jellyfi')