Part Number: PROCESSOR-SDK-DRA7X
Hi Ti Expert:
The readproc tool can convert units into milliseconds,Some operating systems do not have readproc tools,Can you send the readproc tool source code to me?
Or, how can I compile the readproc tool?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PROCESSOR-SDK-DRA7X
Hi Ti Expert:
The readproc tool can convert units into milliseconds,Some operating systems do not have readproc tools,Can you send the readproc tool source code to me?
Or, how can I compile the readproc tool?
Thanks!
Hi,
The source code for readproc is available here: https://git.ti.com/cgit/glsdk/example-applications/tree/cpuload-plugins/readproc.c
Regards
Karthik
Thank you very much for your reply. I'll check it out. If I have any questions, I'll consult you again.
Hi Expert:
I have a few questions. Please help me explain it:
1. 1. Why does the rom_handoff_time variable need to be initialized with __attribute__ ((section(".data"))) ? Why can't it be the same as u32 mmc_init_dur = 0? I don't understand here.
u32 rom_handoff_time __attribute__ ((section(".data"))) = 1;
u32 heap_init_dur __attribute__ ((section(".data"))) = 1;
2. On dra7xx SOC platform, 0x4AE04030 is a 32KHZ counter. If I use TDA4 platform or other platforms, how can I determine the register address of the counter?
#define COUNTER32K_CR 0x4AE04030
3. If the system needs to use uboot during startup, how should we pass the measured time to the kernel?(Not single stage boot)
Thanks a lot!
Hi,
1. 1. Why does the rom_handoff_time variable need to be initialized with __attribute__ ((section(".data"))) ? Why can't it be the same as u32 mmc_init_dur = 0? I don't understand here.
u32 rom_handoff_time __attribute__ ((section(".data"))) = 1;
u32 heap_init_dur __attribute__ ((section(".data"))) = 1;
Can you please provide where you are looking at for this code?
2. On dra7xx SOC platform, 0x4AE04030 is a 32KHZ counter. If I use TDA4 platform or other platforms, how can I determine the register address of the counter?
There is no equivalent counter that runs from SoC power on in the TDA4 platform. You will need to initialize your our TIMER in the bootloader but this will not include the ROM code execution time or until this timer has started.
Hi Expert:
Thanks very much for your reply.
1. Can you please provide where you are looking at for this code?
--> I found it in this link : http://review.omapzoom.org/#/c/38260/5/common/spl/spl.c
2. There is no equivalent counter that runs from SoC power on in the TDA4 platform. You will need to initialize your our TIMER in the bootloader but this will not include the ROM code execution time or until this timer has started.
-->I want to measure the startup time on tda4; (from power-on to kernel startup), how should I measure? Do you have any good suggestions?