This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
MMC2 and MMC3 interfaces are compliant to different standards. MMC2 is compliant with JC64 eMMC Standard (v4.5) and MMC3 is compliant with SDIO v1.0 Part E1. Customer needs to determine if selected eMMC device is compliant with either/both of these standards.
Kalpana,
Is that Micron eMMC chip soldered directly on the customer's PCB? I.e., is it a chip or a card?
thanks,
Kyle
Hello Kalpana,
Can you elaborate on why you can't use MMC2? That interface timing is optimized for eMMC.
Regards,
Kyle