This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Hi
We have a custom board based on the am5718, we have own custom dts and dtsi files, the uboot recognise both SD and eMMC card
=> mmc list OMAP SD/MMC: 0 (SD) OMAP SD/MMC: 1 (eMMC)
but we get the message "no pinctrl state for default mode" when the MLO starts up.
Is it possible to remove this message ?
our .dtsi file looks like this, both the eMMC and SD is feed with 3.3V outside the PMIC
#include "am57xx-industrial-grade.dtsi" … … .. &mmc1 { status = "okay"; bus-width = <4>; cd-gpios = <&gpio6 27 GPIO_ACTIVE_LOW>; /* gpio 219 */ }; &mmc3 { status = "okay"; bus-width = <8>; ti,non-removable; max-frequency = <96000000>; no-1-8-v; /delete-property/ mmc-hs200-1_8v; };
our .dts file look like this
#include "dra72x.dtsi" #include <dt-bindings/gpio/gpio.h> #include <dt-bindings/interrupt-controller/irq.h> #include "dra72x-mmc-iodelay.dtsi" #include "bomill_p2hmi-common.dtsi" … … .. &mmc1 { status = "okay"; pinctrl-names = "default", "hs", "sdr12", "sdr25", "sdr50", "ddr50", "sdr104"; pinctrl-0 = <&mmc1_pins_default>; pinctrl-1 = <&mmc1_pins_hs>; pinctrl-2 = <&mmc1_pins_sdr12>; pinctrl-3 = <&mmc1_pins_sdr25>; pinctrl-4 = <&mmc1_pins_sdr50>; pinctrl-5 = <&mmc1_pins_ddr50_rev20 &mmc1_iodelay_ddr50_conf>; pinctrl-6 = <&mmc1_pins_sdr104 &mmc1_iodelay_sdr104_rev20_conf>; bus-width = <4>; cd-gpios = <&gpio6 27 GPIO_ACTIVE_LOW>; /* gpio 219 */ }; &mmc3 { status = "okay"; pinctrl-names = "default", "hs", "sdr12", "sdr25", "sdr50", "ddr50"; pinctrl-0 = <&mmc3_pins_default>; pinctrl-1 = <&mmc3_pins_hs>; pinctrl-2 = <&mmc3_pins_sdr12>; pinctrl-3 = <&mmc3_pins_sdr25>; pinctrl-4 = <&mmc3_pins_sdr50>; bus-width = <8>; ti,non-removable; max-frequency = <96000000>; no-1-8-v; /delete-property/ mmc-hs200-1_8v; };
Ok, so it is nothing to worry about, thanks for helping me and investigating it
Stefan
Hello Stefan,
In the latest Processor SDK versions this messages started to appear hence its log level was change from debug to printf. To suppress this message you can rename it back to debug and it will appear only when the DEBUG flag is enabled.
Best regards,
Kemal